Relatórios de aplicação sobre a medição de torque
T10F Torque transducer ensures optimization of INVT control algorithm
The Chinese company, INVT, has utilized HBM’s T10F torque transducer and MP60 amplifiers to measure torque and speed of an electric motor controlled by a variable frequency drive (VFD) in order to optimize performance.
Efficient vehicle drives with measurement technology in the original component
Vehicle drives are at their optimum when the drive train and engine control match perfectly. The torque at the transition from engine to gears determines the design of the components. However, there is insufficient space to be...
Long service life and short standstill times with HBM measurement technology
HBM supports highly promising growth markets such as wind energy with state-of-the-art measurement technology. Complete solutions are required to increase the efficiency of wind power plants with HBM measurement technology from...
On test: Generators for wind turbines from The Switch
More precise measurement results with a torque flange from HBM
T40 torque transducer in APL test bench
The independent test bench service provider APL has over 70 state-of-the-art motor and component test benches, and relies on HBM measurement technology.