Artigos técnicos sobre teste & medição
Menores tempos de desenvolvimento graças à testes mais eficientes
A tecnologia de medição de última geração ajuda a indústria automobilística a apresentar mais rapidamente novos modelos no mercado.
Conectar e começar – TEDS: “Plug and Measure” usando identificação de transdutor
A tecnologia “Plug and Play”, que há muito já se tornou um padrão no universo dos PCs, encontrou agora o seu lugar na área de tecnologia profissional de medição. A HBM esteve ativamente envolvida no desenvolvimento da...
On-Site Loading Test of Tunnel Lining Segments in Barcelona
Read how scientists from the Technical University (UPC) carried out loading tests during the construction of the “L9” two-level subway line in Barcelona, Spain. The engineers used a very complex test procedure for analyzing the...
All the president's helicopters: Data acquisition system for rotor blade testing at AgustaWestland
The key criteria of the next generation of presidential helicopters was to ensure the safe transportation of the President of the United States of America, and effectively create an 'Oval Office in the sky'.
A new type of transducer for accurate and dynamic pressure measurement up to 15,000 bar using foil strain gage types
Applications in the ultra-high pressure range are on the move forward. Of particular interest is the manufacturing of diesel injection components such as nozzles and rails.
Displaying results 11 to 15 out of 15