Relatórios de aplicação em teste aerospacial
Lockheed Martin constrói um moderno centro de calibração de transdutor de força (em inglês)
To be sure that their force transducers, despite being economical are still accurate, most aerospace centers take extensive measurements in their own factories. Reliable force transducers are at the heart of structural testing...
Just like real racing: Wind tunnel measurements for simulating the dynamic behaviour of a ground vehicle
Most wind tunnel measurements with ground vehicles are performed with models that are kept stationary during the measurement. With a novel model manipulator, it is possible to simulate the dynamic behavior of the vehicle over the...
Trend assessment for full-scale fatigue testing
Save time and money with real time trend assessment with the new HBM MD Trend software. Full-scale fatigue testing in the aviation industry often takes years to reach the number of flying hours necessary for certification....
Airbus defines a common measurement approach to structural testing
Structural engineers working on the development of modern commercial aircraft can benefit from sharing information, especially when they are located in a number of different countries.
Dassault Aviation: Software offers benefits beyond precision measurement
Dassault Aviation, the French aircraft manufacturer, has improved its test equipment for the development of its Falcon business jets by using HBM's data acquisition and analysis equipment.
Testes estruturais e funcionais na indústria aerospacial MGCplus e catman®Enterprise
- Teste estrutural estático e dinâmico (construção completa)
- Tensão/esforço de componente ou teste de funcionalidade
- Monitoramento e avaliação do desenvolvimento da fadiga
- Análise de tensão de carga estática, fadiga ou durabilidade
- Funcionalidade "ironbird" e teste mecânico
- Testes de trem de pouso
- Testes térmicos e ambientais
- Testes de túnel de vento e aerodinâmicos