Relatórios de aplicação
Electromobility in the fast lane: Efficiency enhancement for the drive of the future
Electrically-driven vehicles have until now been living on the sidelines. But due to ever decreasing oil supplies, increasing fuel prices and a growing environmental awareness, the future belongs to electromobility. In order to...
Reaction times in traffic: an innovative test method using HBM technology
In traffic, it often comes down to a matter of milliseconds. How do we react at the wheel in dangerous situations?With the aid of HBM measurement technology, Swiss engineer Mauro Balestra has developed a way of recreating...
Efficient vehicle drives with measurement technology in the original component
Vehicle drives are at their optimum when the drive train and engine control match perfectly. The torque at the transition from engine to gears determines the design of the components. However, there is insufficient space to be...
Aluminum alloy wheels - tested with QuantumX MX410 data acquisition modules
Shorter development times - this is the aim of all technology companies worldwide. BORBET, the world's leading manufacturer of aluminum wheels shows how it is done: Using a smart system of efficient tests. Always on board: HBM...
Safety in motion - component testing of car seats
C. Rob. Hammerstein (CRH) relies on the S9M force transducer from HBM