Technical Articles on Test & Measurement
Shorter development times with more efficient tests
How latest generation measurement technology helps the automotive industry to gain market presence faster with new models.
Plug in and get started – TEDS: Plug and Measure using transducer identification
Plug and Play has long since become a standard in PC technology. Now it has found its way into professional test and measurement. HBM was actively involved in the development of electronic transducer identification using TEDS...
On-Site Loading Test of Tunnel Lining Segments in Barcelona
Read how scientists from the Technical University (UPC) carried out loading tests during the construction of the “L9” two-level subway line in Barcelona, Spain. The engineers used a very complex test procedure for analyzing the...
All the president's helicopters: Data acquisition system for rotor blade testing at AgustaWestland
The key criteria of the next generation of presidential helicopters was to ensure the safe transportation of the President of the United States of America, and effectively create an 'Oval Office in the sky'.
A new type of transducer for accurate and dynamic pressure measurement up to 15,000 bar using foil strain gage types
Applications in the ultra-high pressure range are on the move forward. Of particular interest is the manufacturing of diesel injection components such as nozzles and rails.
Displaying results 11 to 15 out of 15