arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Keeping an eye on the effects of heavy goods traffic: Long-term monitoring on a motorway bridge

Leibniz University Hannover, germany

Introduction

Increasing heavy goods traffic is a constant endurance test for the approximately 38,000 bridges on the German motorways and main roads. In order to investigate these effects, the Federal Highway Research Institute (BASt) commissioned the Institut für Massivbau (Institute of Concrete Construction) of the Leibnitz Universität Hannover to carry out measurements on a prestressed concrete box girder bridge. Measurement technology from HBK was used over one year to measure e.g. component temperatures, strain and deformation under various traffic situations.

chevron_left
chevron_right

Research project of the Leibniz Universität Hannover

In order to investigate the effects of current heavy goods traffic on the load-bearing structures of a prestressed concrete box girder bridge, the Federal Highway Research Institute (BASt) commissioned the Institut für Massivbau (Institute of Concrete Construction) of the Leibniz Universität Hannover with structural measurements of the box girder structure of a bridge on the A8 motorway. The A8 runs in three segments from the Luxembourg to the Austrian border near Salzburg and is one of the main West-East connections in southern Germany. The following questions needed to be answered:

  • What effects do the increasingly greater total loads of the heavy goods traffic have?
  • What conclusions can be drawn from the determination of the actual traffic compositions on the standard loading evaluations?
  • Must recommendations for the updating of standards be drawn up?

Test setup

The measurements were implemented in three measurement cross-sections where component, internal and external air temperatures, concrete strains and relative deformation were recorded. The strain of the traverses and the deformation of the corresponding lamella between the traverses were recorded at two points on the roadway joints (RJ). In addition, the deformation and movement of the pot bearings were recorded. Laser light barriers were mounted on the existing lateral noise protection walls to detect and determine the speed of heavy goods vehicles. This delivered additional measured values with which the positions of the HGV's in the lanes on the bridge could be determined.

Long distances between sensor and amplifier

In total, the measurement system comprised 96 measurement channels. There were great distances within the structure between sensors and amplifiers. The CANbus system was used to bundle the various measuring points. Four CANHEAD modules with CD 1010 carrier-frequency amplifiers were used here. The measurement channels came together with various connection cards in the amplifier system MGCplus. DC modules, TF modules and connections for PT100 temperature transducers were combined in the MGCplus. In addition to the MGCplus, two Spider8 amplifiers, connected in series to the measurement computer, were connected via the parallel port of the measurement computer. These carried out the deformation and movement measurements for the bearing bodies. Measurement data acquisition was implemented with the software catman®.

Online-monitoring of measurements via GSM

The measurement period was set for one year. As the measurement object is not in the vicinity of the Leibniz University of Hannover, it needed to be possible to monitor the measurements remotely and, where necessary, to influence them. Two GSM modules were integrated in the measurement system for this purpose. One module is used here for separate control of the power supply for the measurement computer and amplifier, the other for the online-monitoring of the measurements.

1.4 GB measurement data per day

The measurement sensor signals are recorded in three measurement rate groups. A measurement frequency of min. 1200 Hz is required for the very short-term actuation of the RJ. Strains and deformations are recorded with 50 Hz and temperatures with 1 Hz. The measurement data with a channel depth of around 100 million measured values runs to around 1.4 GB per day, so that regular monitoring of the system is necessary.

Requirements for a long-term test

The measurement period of one year posed high requirements for the equipment and the settings of the measurement sensors. Therefore great value was placed on the protection of the measurement equipment against weather influences. The sensors on the RJ needed to be protected against penetration of water and de-icing salts in particular as the RJ had become leaky in some areas during the time the structure has been in use. It was necessary to lay the prestressing steels bare at two points to measure the prestressing steel strains. These measurement points were then resealed once installation was complete.

Calibration of the measurement system

Following completion of all installation work and once all measurement procedures were running smoothly, the measurement system on the bridge was calibrated. Various heavy goods vehicle combinations with different total weights were driven over the bridge at different speeds for this purpose. The measurements during the calibration program were used to draw conclusions about the stress based on continuous traffic. Support was provided during this calibration program by Daimler AG in the form of a 25t flatbed truck, a 40t articulated lorry and a 60t vehicle combination based on modular commercial vehicle concept. The motorway bridge was closed to continuous traffic during calibration so that numerous measurement drives were possible.

Leibniz University Hannover

Leibniz University Hannover holds a leading international position in six established key research areas including Biomedical Research and Technology, Quantum Optics and Gravitational Physics, Optical Technologies, Production Engineering, Interdisciplinary Studies of Science and Teacher Training, as well as in the new key research area Energy.

More about Leibniz University Hannover

Jan Peter Liebig

Technology used