Weight Indicators and Weight Controllers from HBM

HBM supplies weighing indicator for all industrial platform scales, truck or container scales. In addition, HBM offers electronic systems for process automation, e.g. for checkweigher and dosing process.

 

 

Digital Weighing Brochure

NO_FILTER
 
  Product   Description
AED Converts the signals supplied by analog load cells into digital data. AED makes Implementation of process control systems easy and convenient.
Converts the signals supplied by analog load cells into digital data. AED makes Implementation of process control systems easy and convenient.
DIS2116 Digital weighing indicator for vehicle scales and railroad track scales
Digital weighing indicator for vehicle scales and railroad track scales
DWS2103 Scale display for communication with legal-for-trade load cells and electronics
Scale display for communication with legal-for-trade load cells and electronics
WE2107 Modern weighing indicator for dynamic and static applications
Modern weighing indicator for dynamic and static applications
WE2108 Legal for trade precision scale electronic
Legal for trade precision scale electronic
WE2110 Precision Digital Weighing Indicator
Precision Digital Weighing Indicator
SLS Battery-operated direct-display SLS scale can integrate into existing suspension systems -available both as legal-for-trade and non legal-for trade
Battery-operated direct-display SLS scale can integrate into existing suspension systems -available both as legal-for-trade and non legal-for trade
RM4220 Amplifier for strain gage transducers with 4 mA to 20 mA output signal
Amplifier for strain gage transducers with 4 mA to 20 mA output signal
VKIA405 Digital amplifier for connecting up to 4 strain gage load cells
Digital amplifier for connecting up to 4 strain gage load cells
SC232/422B Interface converter set
Interface converter set

See related articles on HBM's Weighing Electronics and Indicators

Legal-for-trade weighing systems in open automation applications

Legal-for-trade capability is mandatory in many automation environments. Which components do you need to use to guarantee that your application is legal for trade? For more information, please read our article.

Automatic weighing instruments for legal-for-trade applications: requirements and directives

Weighing technology plays an important role in many industrial applications, for example in bulk material logistics. Depending on the application, different types of automatic weighing instruments are used. What do you have to...

Preventive maintenance of weighing systems

The technological insides of scales have become increasingly complex over the past years. A consequence: When a scale fails, elimination of the problem takes longer and is likely to be more expensive. The better way: Make sure...

Protection against manipulation in weighing technology using 256-bit encryption

Protection against manipulation is among the major challenges in digital weighing technology. HBM relies on extremely secure 256-bit encryption technology. Why this is so and what are secrets behind this technology? You'll find...

Weighing and batching electronics: The Bavarian State Research Center for Agriculture (LfL) relies on HBM weighing technology

Lab-based research studies for optimizing the methane yield and managing the process control of anaerobic digestion of renewable raw materials developed an automatic filling device that continuously loads the fermenter system...

Weighing technology in process plant engineering

How to uncouple a reactor that has to be chilled or heated in the course of a process? What should the approach be if the mixer has to be fitted with a stirrer? How to design the platform if the mixer has to be supported on...