Application Reports on Experimental Stress Analysis

Strain Gauges for a beautiful smile

Strain gauges can be used for measuring almost anything, even strain in braces. Watch our video!

Charpy test: Politecnico di Milano relies on HBM equipment for high speed data acquisition

Italian researchers have selected HBM’s GEN7t high-speed equipment to improve the reliability and accuracy of data acquisition on Charpy tests.

Safe Parachute Opening: Strain Gauges from HBM on board an experimental rocket

Every year a team from the aeronautical association "CLES-FACIL" develops an experimental Rocket in order to research key scientific questions. In a project to calculate the force that is exerted upon a rocket through the opening...

F-35’s performance benefits from BAE Systems integrated structural testing regime

BAE Systems benefits the performance of the new F-35 Joint Strike Fighter through integrated structural testing and derisking the FTI.

US manufacturing utilizes rapid data acquisition to improve production capability

As manufacturing companies across the globe seek to improve the quality of their products, researchers in the USA have utilized HBM’s DAQ equipment to ensure international competitiveness.

Load monitoring in the Olympiahalle arena in Munich

Concerts nowadays, particularly when they involve pop music, are becoming more and more extravagant. Accordingly, the equipment used by the artists for light and sound is large and heavy. As there is a limit to the maximum load...

Setting new records at sea: The fastest sailing boat in the world uses QuantumX

Alain Thébault of France has been pursuing his dream of building the fastest sailing boat in the world for decades. To make this dream a reality, Thébault has consistently relied on leading-edge technologies. When bordering on...

Measurement technology in railway engineering

Extensive testing is required for approval of railway vehicles. This includes complex test runs to measure, for example, the forces between wheel and rail, acceleration in the spring stages or relative displacements of moving...

Spanish university develops tests with HBM equipment for externally reinforced concrete beams

The structural research team at the Universitat Politècnica de Catalunya (UPC), Barcelona, Spain, has developed tests to determine the stresses in concrete beams that are used in construction.

The tests, that have taken the...

DB Minden is testing optical strain gages from HBM

Many tests and inspections are mandatory for approval of new railway vehicles. These include test runs with wheelsets enabling the forces between wheel and rail to be measured. At present, DB Systemtechnik in Minden, Germany, an...

Displaying results 1 to 10 out of 33

1

2

3

4

Volgende

Want to see your application here?

Share a case study of your HBM product with us!

Please contact us