Relatórios de aplicação
Medição de stress residual no método de perfuração (em inglês)
SINT Technology is an Italian firm located in Florence, Italy. The company, in partnership with HBM, produces and develops the MTS 3000, an automatic system for measuring residual stresses by the hole-drilling method.
Optical sensors for lightweights
Modern lightweight materials are increasingly being used in aerospace applications and in other branches, such as traffic and construction engineering, mechanical engineering and the energy business. Fiber composite technology in...
Quando a terra treme ... teste de mesa vibratória com na ZAG
A ZAG Ljubljana, Zavod za gradbeni tvo Slovenije, é o instituto nacional da Eslovênia para construção e engenharia civil onde produtos para construção são testados e certificados.
More safety in buildings: Experimental stress analysis of a passive reinforcement anchorage
An important aspect when designing concrete structures is the precise measurement of anchorage lengths, particularly when
they are positioned in corbels, cornices or load-bearing areas. The connection conditions are...
The signals of an electric eel: piezoelectric power generation on a high-tech bicycle
In the Department of Mechanical, Automotive and Aeronautical Engineering at the University of Applied Sciences in Munich, students are working on an innovative vision of a bicycle. In the
”Electric Eel“ project, the lightweight...