Artigos técnicos
T40B with rotational speed measuring system and reference pulse
Existem no mercado inúmeros sistemas incrementais de medição rotação. No entanto, estes sistemas destinam-se exclusivamente à medição de rotação. Combinar as medições de torque e rotação em um único flange impõe requisitos...
Fieldbus based measurement technology for digital transmission of torque and rotational speed in test benches
Torque and rotational speed measurement equipment must be compatible with the increasing number of fieldbus based systems. Read this article to learn how T40B and T40FM digital torque transducers meet these requirements.
Measuring torque in wind energy applications
There is no power generation without rotation, hence, there is no power without angular speed and torque: This applies to wind energy in particular. This article highlights the importance and significance of measuring torque in...
The right fit for your torque transducer
Correct torque application to the transducer is crucial for measuring torque. We show you what to keep in mind when selecting a fit.
Checking HBM torque flanges using the shunt signal and the zero point
Torque transducers need to be calibrated before being put into operation. A practicable method is to determine the characteristic curve of the transducer using a zero point value and a second reference value based on the shunt...
Use of torque flanges in power generation plants
Power generation plants need to be economical and eco-friendly. To determine the efficiency of such plants, drive power needs to be measured. However, which method is most suitable? Read this technical article to learn how to...
The right coupling for your torque transducer
Couplings are an important accessory for torque transducers. This article provides you with important information on which factors you should consider when choosing the coupling that best fits your application.
Power measurement on large drives with combustion engines
There are different ways to measure the power of large drives with combustion engines. Learn how direct power measurement in the drive train reduces the uncertainty of measurement, by contrast with indirect measurement on the...
Measuring torque in marine propulsion systems
An efficient ship drive control includes measurement technology directly in the drive train. HBM torque flanges contribute to optimizing the performance of ship drives.
High Precision Torque Measurement System
The subject of the paper is the development of a contactless torque measuring system with a carrier-frequency amplifier.