Practical tips for working with catman®
catman® is the powerful software for acquiring, visualizing and analyzing your measurement data. To enable you to benefit even more from using catman® for your measurement tasks, we have prepared some practical examples for catman®AP and catman®Professional.
catman® Practical Examples
catman®AP / catman®Easy with EasyScript module: How to write test values during an ongoing measurement to an Excel file?
EasyScript example (for catman®Easy): Single values (Snapshot) to Excel
How to analyse a decay curve in catman®Professional?
The time period (delta t) between two defined points (e. g. 80% and 20% of the maximum) is to be computed for a decaying signal variation (e. g. cooling curve). In catman® Professional this task can be solved using an Auto...
catman®Professional: How to use the ActiveX library of catman in Visual Basic?
Example program for using the ActiveX library of catman in Visual Basic. For
How to connect catman®Professional and Excel with ActiveX?
This Excel macro generates a catman object and starts through catman a data acquisition of 100 values from the first channel.
Knowledge Base for catman®Professional
The catman® knowledge base is a collection of technical articles covering the catman® software package for data acquisition and analysis.
Click here to download the catman® knowledge base
Suited up to catman®Professional version 5