Case studies on agriculture
Idento Operations uses HBM load cells for intelligent feed systems
Idento from the Netherlands makes special measuring units for weighing feed quantities for pigs and cattle. Idento uses hermetically-sealed load cells from HBM for its measuring units, and they have turned out to be able to...
Usada na maior região vitivinícola da Austrália: Célula de carga universal Z6 da HBM
Alta umidade do material processado e, ao mesmo tempo, altas temperaturas: A empresa australiana Accuweigh conta com tecnologia de medição HBM diante das difíceis condições de um centro de compostagem.
Eletrônica de pesagem e de dosagem: O Centro de Pesquisa para Agricultura do Estado da Baviera (LfL) conta com a tecnologia de pesagem HBM (em inglês)
Lab-based research studies for optimizing the methane yield and managing the process control of anaerobic digestion of renewable raw materials developed an automatic filling device that continuously loads the fermenter system...
Too much fertilizer? A globally unique test bench for investigation and analysis
Cemagref, the French Institute for Agricultural and Environmental Engineering Research is a specialist in spreading fertilizer at one of its nine sites in Montoldre. The equipment to chart the spread of the fertilizer as it is...
Análise de grãos inteiros com tecnologia de pesagem HBM
Cereais e grãos são produzidos no mundo inteiro.
Want to see your application here?
Share a case study of your HBM product with us!