- Transdutores & Sensores
- Eletrônica de medição
- Strain gages & acessórios
- Componentes de Pesagem
- Calibration & Services
![]() |
|
|
GEN7t/16t - High speed / high channel count DAQ
and transient recording for high end requirements
|
|
|
Complex technical systems can only be controlled if they are known in detail. Obtain a perfect overview of your system with the GEN7t/16t. With GEN7t/16t, you can configure up to 1,080 synchronized channels according to your requirements. Your system grows from the first channel onwards exactly as your project changes. Stay on top, rapidly, reliably, flexibly and always with perfect precision. Up to 8 GEN "slaves" can be connected to a GEN7t/16t master, each of these 9 devices can contain between 4 and 120 channels, and all 1,080 channels can measure in synchronization with each other. Scale your system as precisely as you require it. Click here to download the GEN7t/16t brochure (PDF)High-speed laboratoryGEN7t/16t captures and records interference peaks with a sampling rate of up to 100MS/s. On all channels if necessary! It is possible, with the Dual Rate Recording principle, to record fast transients and, at the same time, record a continuous measurement series on the same channel. This means that long-term observations can be continuously recorded at 10MS/s while, at the same time, rapidly occurring events can be recorded with a sampling rate of 100MS/s, trigger-controlled. World champion level in all disciplines - GEN7t/16t plays in the top league
Gigabytes in seconds: Precisely recorded with 100MS/s – saved in secondsGEN7t/16t records gigantic data volumes within just a few seconds. Save directly to your PC hard drive, a removable disk or network server via Gigabit Ethernet. Professional storage modes such as "Streaming to disk" or continuous circular recording on disk help in this process. To ensure that no samples get lost, an SCSI RAID can be optionally connected. Or, if it needs to be quick, RAID 0 for even faster data storage. Transmission rates:
Observe your data even before the end of the actual test. Or zoom into the details of your data. The software supports numerous display options. Input amplifier for each sensor - selectable via softwareComplex systems contain all types of signals. Sensor type and input circuits must match each other. GEN7t/16t provides the entire spectrum of physical input amplifiers, you just need to select the appropriate one using the software, whether they are bridges, differential connections, resistance-based for current measurements or optimized for ICP® piezo sensors. Immune against electromagnetic interferencesOptionally, galvanically isolated input amplifiers are also available. They protect the measured values from interference signals such as those that occur in the vicinity of large machines or in the high voltage sector. For precise transient recording:
For strain gages
For CP® piezo sensors, resistance-based current measurements or galvanically isolated measurements
For fast peaks, when speed counts
For binary and frequency signals, e.g. from position encoders
Transportable in tower or stationary in 19" housing for control cabinet mounting High-speed 19" laboratory for installation monitoringThe GEN16t fits directly into standard 19" control cabinets, as normally found in production systems. Measurement technology with peak perfection is the core competence of the GEN16t. In contrast to high end VXI and VME systems, GEN7t/16t contains the complete software required for immediate start. Measuring points can be configured without programming with this software. Communication with the central computer is via Gigabit Ethernet (Cat 5e UTP). Measurement intelligence at the event location - limitless without ground loopsDistributed measurement intelligence means measuring spatially separate but synchronously. All channels in all connected GEN7t / GEN16t are synchronous with one another. The optical synchronization concept makes it possible to create measurement sites with several GEN7t/GEN16t over distances of several hundred meters without ground loop issues. Equipped for the futureThe flexible concept behind GEN7t/16t also includes all options for future tasks. Profit from the simple upgrade possibilities of the master/slave concept. GEN7t/16t grows with your tasks, flexible, precise, without limits from the first to the 1,080th channel. Despite the high complexity, configuration and commissioning are simple. The supplied software ensures this. Your requirements keep growing - and GEN7t/16t grows with themAlmost unlimited: Your task determines how your measuring instrument is set up and not vice versa. Simply plug in the next card, configure, connect and away you go. The software helps you. Total Cost of Ownership (TCO) means having all costs incurred in view. This includes all costs, whether from familiarization, installation, operation or maintenance. Give your budget a break and save money with the versatile and flexible upgrading options. Versatile in use:
GEN7t/16t at a glance
GEN7t/16t only differ in their mechanics. GEN7t
GEN16t
Typical applications:
Typical application areas:
Communication:Interface: Transmission speed: Measuring device:
|