arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Teltek dynamic scales for the right quantity of fish in the pack

teltek, Sweden

Introduction

HBK's intelligent load cells measure on the go when the production process cannot stop

Teltek makes process monitoring equipment for the food and drink industry and is the only Swedish manufacturer of dynamic scales, making them experts at weighing products as they move. They have just supplied a new in-house scale to a fish factory belonging to frozen food manufacturer Espersen in Lithuania. It will be an important part of the production line, ensuring that every pack of frozen fish contains the labeled quantity of cod, pollock or mackerel fillets – no more and no less. The job of HBK's load cells in the new scale is to guarantee accurate weighing despite the high production speed and the challenging conditions in the fish factory. "For our customer – a fish producer – it is very important for the weight of the pack to be as close as possible to the labeled weight. If the weight is too high, the producer stands to lose a lot of money. And if packs are under weight, they may be in conflict with directives of the Swedish National Food Administration", explains Tomas Moqvist, MD at Teltek.

chevron_left
chevron_right

Rapid sorting and weighing

Teltek, based in Örebro, Sweden, develops, designs, programs and installs dynamic scales, primarily in the food and drink industry but also in other sectors like chemicals and hardware (weighing screws as part of the verification process). Virtually all the scales supplied by Teltek are tailored to meet customer requirements. The scale supplied to the fish factory was designed to sort incoming fillets of fish for packing in 400 gram units, at a rate of approximately 55 packs per minute. This is about what two people can manage when working at the conveyor.

Digital load cells are the key

Teltek's approach involved six parallel buffer plates on each side of the scale, with room for a total of twelve fillets that have passed through the two fish sorters. A combination of fish fillets is selected to come as close as possible to the target weight of 400 grams per pack. The central components of the machine are the six digital HBK PW15AHi single point load cells, with a pneumatic motor to advance the belt. "Obviously, the primary function of the machine is weighing, but a lot of thought went into how the fish is handled and transported – this is a delicate raw material that can easily fall apart. We clearly want to keep waste to a minimum", says Tomas Moqvist, who has learned a lot about raw fish during the project.

Built-in intelligence

Unlike many other scales, in which Teltek uses a combination of analogue load cells and in-house filters, the decision was made to use digital load cells in the new fish scale. As a result, a certain amount of intelligence could be built into the load cells directly, for example signal filtering functions.

Dynamic weighing is a big challenge

Communication and data transmission from the machine is based on the standard serial interface protocol, RS485. The scale is operated from a user friendly touch screen next to the machine. The underlying computer program and the algorithm controlling the choice of fish fillets for each pack were developed in-house by Teltek. The program tests all the various combinations of the 12 fish fillets on the scale, selecting the best match for each pack. The whole process takes about a second, using a lot of computer power. "Most load cells on the market are intended for static applications. High speed dynamic weighing is a different ball game. HBK is the only manufacturer who is talking about dynamic features in load cells, and also the only one putting so much effort into product development relating to dynamic weighing. It's important for us to work with a manufacturer who is at the cutting edge", explains Tomas Moqvist.

Handling the rough stuff

The wire strain gauges in the load cells are sensitive to moisture, so they need to be designed to withstand the challenging conditions in the fish factory, where the machinery is cleaned with a strong jet of water several times a day. The load cells are therefore made of stainless steel, and installed in a protected box that is kept under pressure to repel moisture.

Aiming for reliability

It's a big problem if the machine stops working. More fish arrive on a daily basis, and they need to be processed. Reliability and ease of maintenance of the components are crucial. "The HBK load cells we use in the fish scale have the highest level of moisture protection, IP68. The original load cells in one of the first fish scales to be delivered worked perfectly and are still going strong after two years of demanding double shifts. We've done some fine tuning in the new machine, and we're aiming for reliability that is at least as good", says Tomas Moqvist in conclusion.

About Teltek

  • Makes process monitoring equipment for the food and drink industry
  • Experts in dynamic weighing
  • Founded in Örebro 1982
  • Thousands of checkweighers installed with customers
  • First in Sweden to receive type approval for a dynamic scale (1993)

More about Teltek

Technology used