arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

PW22 load cell meets requirements of scales manufacturer and certification body

Simionato, HayssenSandiacre, ITALY

Introduction

Number of weighing operations in multi-head weigher doubled

In 2006, HBK developed the PW22 single point load cell in cooperation with the Italian company Simionato, producer of linear, batching and multi-head weighers combined with vertical packaging machines. HBK produced various prototypes, certified the load cell and made possible the industrial manufacture of the product with several measuring ranges. The load cell is still successfully in operation and allows to double the number of weighing operations.

chevron_left
chevron_right

Specially developed for use in multi-head weighers

Simionato placed high demands on the load cell's properties: “The PW22 load cell has been designed by Simionato and HBK specifically for RCW Simweight multi-head weighers. It meets all the precision, speed and thermal stability requirements of the OIML R60 international recommendation for load cells”, explains Francesco Renzulli, responsible for the Metrology Sector. However, the load cell not only had to fulfill Simionato's requirements. OIML criteria had to be met as well. The OIML recommendation indicates the specifications a load cell must meet to be considered conforming to static and automatic weighing system requirements. The PW22 load cell has been certified by one of the most recognized accredited laboratories in Europe with a reputation for being also one of the most severe in terms of regulatory compliance.

PW22 for dynamic weighing

HBK's PW22 load cells are competitive products offering the very highest performance compared to other OML R60 certified load cells on the market. The load cell has a minimum verification interval of 0.5 g and 6 kg maximum capacity, with a guaranteed 12,000 real reading points. This high level of sensitivity means that a multi-head weigher can be homologated with a scale division of +/- 0.5 g.

Number of weighing operations doubled

The Simionato R&D division also tested the settling times (reading speed and result stability), which were half that of competitors' load cells. Thanks to their fast reading times, multi-head weighers fitted with PW22 load cells can perform twice as many weighing operations as other multi-head weighers on the market. The temperature chamber test was equally important. It confirmed compliance with the zero and gain drift required by OIML R61-1.

More certifications will follow

As well as having been certified by PTB, the PW22 has been tested by accredited laboratories (EUROTEST and CERMET) in all the Metrology tests during the homologation of the Simweight multi-head weighers and the new ATOM line. The RCW will soon also be MID (Measuring Instruments Directive) certified.

Simionato Integrated Packaging System srl

Simionato has been developing and producing linear, batching and multi-head weighers combined with vertical packaging machines since 1963. The combined offer makes the Simionato solution unique. The company takes pride in the constant innovation of fully-functional packaging systems. Today, Simionato is part of the HayssenSandiacre Group, and can develop an even wider range of machines and services.

More about Simionato

HayssenSandiacre

HayssenSandiacre is a world leader in FFS technology and services. Its VFFS and HFFS (Vertical and Horizontal Form Fill Seal) machines are innovative and extremely fast, filling and packaging thousands of foodstuffs and a wide range of other products for the industrial, institutional and retail distribution sectors. HayssenSandiacre is based in Greenville-Spartanburg, South Carolina. The company is part of the Barry-Wehmiller Group, the top automated packaging group in the western world.

More about Hayssensandiacre

Technology used