Application Reports on Industrial Process Control

CODESYS Application – Communication catman AP - PMX

This is a guide to create a CODESYS application for PMX from HBM.

PMX Tolerance-window

This is an instruction for creating a tolerance-window in the PMX that can be used for a component or performance test for example.

New application possibilities for innovative torque measurement in test benches – with PMX

Torque measurement plays an important role in engine test benches. Read this technical article describing how to implement efficient control and automation, in addition to maximum accuracy and speed.

Vibration damping of ultra-light belt conveyor galleries

HBM force transducers are applied in a research project to reduce vibration in ultra-light belt conveyor galleries. Read this case study to learn more about the project - from the model to full implementation.

Ricoh improves toner cartridge manufacture for latest product

Ricoh UK Products Ltd has worked with Mechatronic Solutions and HBM in developing a one-piece assurance system for the automatic assembly of its latest toner product for the European market.

Machine condition monitoring using PMX

Component parts in rolling mills are subjected to high stress. If e.g. bearings wear out prematurely, product quality decreases. Since this happened at a manufacturer of aluminum products, SKF decided to use HBM's PMX amplifier...

Smart devices undergo intensive testing

Modern smartphones and operating units provide fascinating new features and user friendly design. But these devices must pass through an extensive development and testing process before they ever reach consumers.

Quality control for switching devices

Switching on and off reliably – over the entire service life of a switching device. Guaranteeing this is the task of end-of-line test benches in switching device manufacturing.

Press monitoring boosts operating time

Modern industrial production would be unthinkable without presses. The range of products extends from coins to large automotibile parts. Presses run at up to 800 strokes per minute. The quality of the workpieces that are produced...

Top-qualitiy steel - reliably recording all parameters

Depending on the final product, steel must be available in a special shape, alloy and quality. The quality of the outgoing products, sheet steel, is largely determined in production.

Displaying results 1 to 10 out of 34

1

2

3

4

Nästa >

Want to see your application here?

Share a case study of your HBM product with us!

Please contact us

Select by Signal Conditioner