Technical Articles on Torque Measurement
Which fit is the right one?
An explanation of the significance of ISO fits to standard shafts and holes
Checking HBM torque flanges using the shunt signal and the zero point
Users often ask whether they may continue using a torque flange that has not been in use for an extended period of time.
The use of torque flanges in power generation plants
Power generation plants need to be economical and eco-friendly. To determine the efficiency of such plants, drive power needs to be measured. However, which method is most suitable? Read this technical article to learn how to use...
Couplings and mounting parts for torque applications — a selection guide
Which coupling is the right one?
A torque flange is a precision transducer that enables very small uncertainties of measurement to be attained. However, to achieve this special requirements need to be met. It is most important...
Power measurement on large drives with combustion engines
There are different ways to measure the power of large drives with combustion engines. Learn how direct power measurement in the drive train reduces the uncertainty of measurement, by contrast with indirect measurement on the...