HBM measurement technology in the automotive industry

Be it in production, quality control or research and development - HBM measurement technology is used in a wide range of applications in the automotive industry. Move the mouse over the individual car components to view detailed information about our measurement solutions for your application.

Choose a field of application:

Application reports from the automotive industry

Serving a greener automotive industry

The demands on energy efficiency and the CO2 balance of motors are constantly increasing. A manufacturer of water, oil and vacuum pumps for thermal engines therefore decided to use a complete solution from HBM.

Testing of electric and hybrid cars: HBM, a key partner for the French company, GreenMot

Tests on electric motors present a new challenge when it comes to measurement. French testing company GreenMot has opted for HBM's innovative eDrive testing solution.

HBM on the test bench: Allison Transmission puts HBM to the test

Allison primarily uses HBM products to handle dynamometer driveline torque and speed measurements for hybrid electric development, powertrain development test stands. They currently use the T10F torque flange, T32 FNA torque...

Better driving thanks to PME

For testing seat mountings and even complete car seats, Kühne + Vogel have already developed and produced a number of machines for famous automotive suppliers. The deciding quality criterion for user comfort in a car seat is the...

Reducing the cycle time with FASTpress when assembling cylinder heads

In combustion engines, valve seats and valve guides are subjected to special loadings. There are thermal loads as well as mechanical loads, produced by the ignition pressure or by the valve disk coming down hard when closing....

Volvo Construction Equipment (CE): Making loaders more fuel-efficient with toughest tests - and SoMat eDAQ data acquisition

Volvo Construction Equipment (CE) uses HBM's SoMat eDAQ test system to help it test loader prototypes under extreme conditions.

Electromobility in the fast lane: Efficiency enhancement for the drive of the future

Electrically-driven vehicles have until now been living on the sidelines. But due to ever decreasing oil supplies, increasing fuel prices and a growing environmental awareness, the future belongs to electromobility. In order to...

Reaction times in traffic: an innovative test method using HBM technology

In traffic, it often comes down to a matter of milliseconds. How do we react at the wheel in dangerous situations?With the aid of HBM measurement technology, Swiss engineer Mauro Balestra has developed a way of recreating...

Efficient vehicle drives with measurement technology in the original component

Vehicle drives are at their optimum when the drive train and engine control match perfectly. The torque at the transition from engine to gears determines the design of the components. However, there is insufficient space to be...

Aluminum alloy wheels - tested with QuantumX MX410 data acquisition modules

Shorter development times - this is the aim of all technology companies worldwide. BORBET, the world's leading manufacturer of aluminum wheels shows how it is done: Using a smart system of efficient tests. Always on board: HBM...

Displaying results 1 to 10 out of 36

1

2

3

4

Nästa >

Measurement solutions for development, production, testing and calibration

HBM Solutions for the Automotive Industry

Products & Services

Application Reports