MGA Amplifier

MGA II - Amplifier system devices with Eurocard modules

Product Description

MGA II modules

DA12: Digital indicator with 4 1/2 digit LED display complete with differential input. Designed as a digital voltmeter for displaying output voltage, switchable over 12 channels, with controllable decimal point and overflow LED.

ME10, DC: DC voltage amplifier for high frequency measurement processes, for connection to strain gauge transducers. With a maximum measurement frequency of 10kHz and a very short settling time, the ME10 is particularly suitable for dynamic measurement processes, such as in the case of rapid variations in forces during punching or press-fit tasks.

ME30, 600 Hz TF: An amplifier for use with strain gauge transducers during low-frequency measurement processes. Its good zero-point stability enables it to be used in static and quasistatic measurement processes such as e. g. weighing and dosimetry, or the measurement of forces and pressures in industrial test rigs.

ME50, 4.8 kHz TF: An amplifier for transducers with inductive half bridges, such as the HBM range of displacement transducers. The ME50 can be used for static and dynamic measurement processes, such as long-duration monitoring in construction measurement technology.

ME50S6, 4.8 kHz TF: Amplifier for strain gauge transducers. Like the ME50 (for inductive half bridges), the ME50S6 is suitable for such applications as force vs. displacement measurements.

EM001: This optional, connection-board mounted final stage module is switchable between a current output of ± 20mA or +4 to +20mA, and a voltage output of ± 10V (R > 500Ohm).

EM002: Output stage module for Euro cards (± 20mA, 4...20mA)

AP01: Standard connection board for transducer connection using Sub-D connectors.

AP03: Connection board for transducer connection using 7-pin MS connectors.

AP11: Connection board for transducer connections using Lemo sockets.

Housing: Depending on the application, there is a choice between desktop housings for 6 channels and a rack frame with capacity for 12 channels.

ePLAN

In addition to the industrial amplifiers HBM provides the appropriate ePLAN macros. They allow easy and error-free integration of the instruments in the project planning of the automation environment.

ePLAN Electric P8 is an engineering tool for modern CAE software supported by a database and facilitates consistent project planning, documentation and administration of automation systems. ePLAN macros enable users to easily integrate the process controllers in their project planning. Parts data, drawings and pin assignments are available in ePLAN Electric P8 immediately after import of the macros.

The free macros are available on the documentation CD included in the process controllers' scope of supply and can also be downloaded here.

Product Literature

Vänligen ange din epostadress.

Logga in här med hjälp av din epostadress om du redan har ett konto på HBM.com och få tillgång till HBMs kompletta tekniska dokumentation.
MGA II

Data Sheets

ENDEESFRITPTCNJPKR
Data SheetPlease log inPlease log inPlease log inPlease log in

Operating Manuals

ENDEESFRITPTCNJPKR
Operating ManualPlease log inPlease log inPlease log in
Operating Manual ME10Please log inPlease log inPlease log in
Operating Manual ME250 S6Please log inPlease log inPlease log in
Operating Manual ME30Please log inPlease log inPlease log in
Operating Manual ME50Please log inPlease log inPlease log in
Operating Manual ME50S6Please log inPlease log inPlease log in

Case Studies

SCHULER: HBM measurement technology in process monitoring

The force of the pressure used for minting is crucial for the quality of a coin. SCHULER relies on HBM measurement technology for monitoring forces in coining presses.

Serving a greener automotive industry

The demands on energy efficiency and the CO2 balance of motors are constantly increasing. A manufacturer of water, oil and vacuum pumps for thermal engines therefore decided to use a complete solution from HBM.

Utilizing strain transducers for greater accuracy in forging

One of the world's largest automotive component suppliers, Hirschvogel Automotive Components, based in Pinghu, China, is utilizing HBM’s SLB strain transducer and MP55DP amplifier system to monitor forging forces for improved...

It all comes down to the right quantity of force

The more precisely powder presses can apply force, the higher the quality of the produced molded parts. The pressure must be accurately measured for exact control. Dorst Technologies has elected to use HBM's PMX amplifier...

HBM on the test bench: Allison Transmission puts HBM to the test

Allison primarily uses HBM products to handle dynamometer driveline torque and speed measurements for hybrid electric development, powertrain development test stands. They currently use the T10F torque flange, T32 FNA torque...

Better driving thanks to PME

For testing seat mountings and even complete car seats, Kühne + Vogel have already developed and produced a number of machines for famous automotive suppliers. The deciding quality criterion for user comfort in a car seat is the...

One for all - Universal hydraulic test bench with secondary control

Until now, hydraulic test benches were designed for special tasks or products. Although the individual components are already tested, the interaction between individual pumps and control systems can only be tested in the machine...

Measured force on the chain

Hoisting technology is one of the applications for the chains produced by the company Ketten Wälder GmbH. The processing of the base materials, such as steel for the chains, is a complex process, and all the sequences have to be...

Machine monitoring made easy

Artis GmbH in Bispingen is an international leading company in the sector of tool, process and machine monitoring. Artis is using the proven piezoelectric systems of the HBM Paceline series in the monitoring of turning-turning...

Safety in motion - component testing of car seats

C. Rob. Hammerstein (CRH) relies on the S9M force transducer from HBM

Displaying results 1 to 10 out of 33

1

2

3

4

Nästa >

Request a Quote!

Tack för att du visat intresse för HBMs produkter. Med hjälp av detta formulär kan du enkelt skicka din offertförfrågan.