Adhesives & Bonding Material
The most common way in which strain gages are attached to measured objects is by bonding.
HBM adhesives meet the following requirements:
- transmission, as much as possible without loss, of the deformations of the measured object to the strain gages
- stable behaviour across a temperature and strain range which is as wide as possbile
- strain gage and measured object must not be chemically attacked.
Your criteria for adhesive selection should be:
- application temperature
- material of your workpiece and recommendations for the relevant strain gage
- requirements for long-term stability and reproducibility