技術文章
從市場領導者處獲得專家建議...
基礎知識,應用案例,產品資訊 – 來自 HBM 多篇技術文章 可以為你的試驗應力分析提供幫助.
The industrial benefits of utilizing well-proven strain gauges
Well-proven foil-type strain gauges have many advantages over alternative technologies believes HBM's Dr.-Ing. André Schäfer
Successfully compensating for lead resistances
If measuring points are not directly accessible, the measuring instruments need to be connected using long cables. The disadvantage: The lead resistance can negatively affect the measurement. Various types of strain gauge...
Metrological recording of deformation development in ultra-high performance concrete (UHPC) in a triaxial test cell
This article shows that by using a "triaxial cell" test rig, it is possible to determine the triaxial strengths for both static and dynamic loadings.
Using statistical techniques to validate field test data for fatigue analysis
This paper describes some statistical techniques for taking measured data and projecting what the expected time history and resulting fatigue damage would be if test data were collected for much longer times.
Early warning of damage to wind turbine rotor blades
Suitable sensor technology must be employed to detect the damage to wind turbine rotor blades early enough, and minimize the economic consequences. The sensors must be able to withstand tough ambient conditions and must...
Improved Strain Gage for Residual Stress Analysis Using the Hole Drilling Method
In the following it will be demonstrated that the new HBM symmetrical rosette design will significantly reduce the errors in the measurement and will allow much more reliable stress results.
Measuring surface strain using flexible fiber-Bragg strain gauges
Our comprehensive article provides basic knowledge on the topic: Everything you need to know about measurement using optical strain gauges: From technological background information through calibration of interrogators and...
Installing strain gauges on fiber-reinforced composites
Fiber-reinforced composites are used in an increasing number of applications. These materials too can be tested using strain gauges, which is shown in this article.
Selection and models of strain gages (SGs)
SGs are selected depending on the measurement task by model, series, connection type, temperature response adaptation, active measuring grid length, and electrical resistance. In terms of the application, the model of SG that is...