提高稱重測量的信心: 技術文章,訣竅和技巧
為了提高稱重測量的精度和耐用性,很多方面需要考慮,包括安裝,評估和使用稱重感測器等等。
我們的技術文章為您提供了如何 正確使用,安裝 稱重感測器的各種 技巧和資訊。
稱重測量基本知識
Structural Design of Tank Weighing Systems
Some essential rules must be followed when installing load cells in tanks. Typical tank designs are represented in a stylized manner by way of example.
Overload protection - good protection for load cells
The constructive outlay of a specially designed overload protection is always justifiable when the load cells need to be loaded up to their maximum capacity, where the risk of overload is always present. Overload protection...
Utilization of weighing modules for load cells to avoid incorrect loading
Incorrect loading of load cells can be avoided utilizing adequate mounting parts. The load cell and the mounting part together form a complex functional unit, a weighing module for load cells. HBM weighing modules come...
Load application in load cells - Tips for users
Correct load application on the load cells is a prerequisite for precise weighing results. Be it load direction, support structure or mounting aids – load application is influenced by multiple factors.
How does a bending beam load cell work?
Bending beam load cells are the most widely used types of load cells. Read this article to learn more about the benefits and properties of bending beams.
稱重測量的標準和認證
The virtual truck scale: new trends you should take note of
Legal requirements to be complied with when operating truck scales are becoming increasingly demanding and can only be met using cutting-edge weighing instruments. Our interactive animation shows what needs to be taken into...
IP69K: the highest degree of protection possible at present. Video available!
When load cells are used in harsh environments, the right degree of protection is crucial. HBM offers load cells up to the highest degree of protection IP69K. Our video demonstrates how much a load cell needs to tolerate ...
The ATEX certificate - explained interactively
Adequate explosion protection plays a crucial role in many applications. Our interactive animation shows you how to correctly read an ATEX certificate.
Accuracy classes - in simple terms
C3, C6, ... What is the significance of the different accuracy classes - and what accuracy is required for what application? Our survey provides useful help.
Well shielded: EMC-tested weighing equipment
Be it in packaging machinery or filling systems- load cells always need to weigh precisely and be easy to integrate. Weighing equipment affecting other technical devices through unwanted electrical effects - or vice versa...
Protection against manipulation in weighing technology using 256-bit encryption
Protection against manipulation is among the major challenges in digital weighing technology. HBM relies on extremely secure 256-bit encryption technology. Why this is so and what are secrets behind this technology? You'll find...
Load cells under test: many promise C6, but few deliver
C6 accuracy is often promised - however, it is not always attained. This article shows you how you really get the quality you need for your weighing technology application.
在生產過程中使用數位稱重技術
Legal-for-trade weighing systems in open automation applications
Legal-for-trade capability is mandatory in many automation environments. Which components do you need to use to guarantee that your application is legal for trade? For more information, please read our article.
Automatic weighing instruments for legal-for-trade applications: requirements and directives
Weighing technology plays an important role in many industrial applications, for example in bulk material logistics. Depending on the application, different types of automatic weighing instruments are used. What do you have to...
Preventive maintenance of weighing systems
The technological insides of scales have become increasingly complex over the past years. A consequence: When a scale fails, elimination of the problem takes longer and is likely to be more expensive. The better way: Make sure...
Standardization or customization?
To succeed in today's fierce global competition, companies are always looking for new ways to make their processes more efficient. Quality assurance through effectively monitoring filling and batching processes using modern...
無菌稱重
Clean, accurate weighing: hygienic design is worth it
Hygienic design is a major trend in food processing technologies. This article explains how to benefit from efficient and clean load cells for assuring hygienic processes across the complete production line.
No chance for bacteria or dirt
Clean foods and medicines are essential when health is in question. Production is becoming increasingly automated; a trend that is also the case for plant cleaning. It becomes increasingly important for the design of the plant’s...
Hygienic design is mandatory
Hygiene plays a decisive role in an increasing number of applications in the food industry. This article provides basic considerations on the topic
Clean solution: hygienic system design with HBM load cells
Hygienic system design in weighing technology: HBM's new hygienic load cells play a particularly important role in this context. Read the article to learn what to keep in mind