Structural health monitoring with HBM

結構監控: 為你提供可靠的測量結果

用於建築物規劃,設計,以及災害評估或者進行疲勞測試: 我們能夠為結構安全監控提供可靠的測試結果.

結構安全監控的產品和服務

一座橋樑是否能夠永久使用? 建築物能否修復? 當某個部分改變或移除情況下,整體結構是否能夠保持? 特定的建築材料是否能符合要求? 地震測試是否能夠模擬?

如何能夠瞭解結構的真實狀態,進行安全監控?答案是採用 HBM 的產品和服務: 包括 應變片, 感測器, 放大器測量軟體 均來自單一源 — 能夠滿足你結構測試的所有測量要求。 我們同時還提供專業的服務,包括現場安裝,調試和維護。

如果你對結構安全監控有任何問題,請聯繫HBM

無論是需要測量 壓力,位移,力,溫度,振動還是加速度還是結構安全監控的其他物理量: HBM 的感測器和放大器都能為你提供值得信賴的測量結果transducers .

HBM 用於結構安全監控 的測量技術能夠為你在結構規劃,設計,建造以及在長期監控方面提供幫助,包括:

  • 建築
  • 橋樑
  • 水壩
  • 隧道
  • 道路

HBM 關於結構安全監控的應用報告:

Static and dynamic load tests completed in record time: SHP opts for QuantumX from HBM for bridge monitoring

Only five days were allowed for static and dynamic load tests on a new bridge across the Nitra river to be conducted by the Czech company SHP. One of the secrets behind the success: utilization of HBM's QuantumX data acquisition...

Optimal dosing always in view: RTN installation modules in a new CEMEX Austria binding material silo

In order to ensure optimal mixing and dosing of the material anhydrite flow, CEMEX Austria is using HBM weighing technology for their new binding material silo.

Underwater blasting project meets stringent safety limits with HBM’s Genesis equipment

Two US contractors have used HBM's Genesis high-speed data acquisition equipment to successfully monitor the underwater blasting of a one-mile long, environmentally-sensitive section of the Columbia River near St Helens in...

Load monitoring in the Olympiahalle arena in Munich

Concerts nowadays, particularly when they involve pop music, are becoming more and more extravagant. Accordingly, the equipment used by the artists for light and sound is large and heavy. As there is a limit to the maximum load...

Keeping an eye on the effects of heavy goods traffic: Long-term monitoring on a motorway bridge

Increasing heavy goods traffic is a constant endurance test for the approximately 38,000 bridges on the German motorways and main roads. In order to investigate these effects, the Federal Highway Research Institute (BASt)...

Load testing on the Ponte della Costituzione in Venice

The Ponte della Costituzione is designed by the Spanish architect Santiago Calatrava and became the fourth bridge over the Grand Canal in Venice when it was inaugurated in September 2008. HBM Italy worked with Verona-based Veneta...

Tunnel monitoring with QuantumX and catman®Script in the Aescher tunnel in Switzerland

The monitoring of structures makes an important contribution to their reliability.

Tunnel monitoring with QuantumX and catman®Script in the Aescher tunnel in Switzerland

The monitoring of structures makes an important contribution to their reliability.

When the earth rocks... vibrating table tests at ZAG

The ZAG Ljubljana, Zavod za gradbeni tvo Slovenije, is Slovenia’s national Institute for building and civil engineering, where building products are tested and certified.

More safety in buildings: Experimental stress analysis of a passive reinforcement anchorage

An important aspect when designing concrete structures is the precise measurement of anchorage lengths, particularly when

they are positioned in corbels, cornices or load-bearing areas. The connection conditions are...