能源工業
HBM - 能源工業的閤作伙伴
隨著全球能源需求的持續增長,確保產品結構的安全性,包括功能,以及性能的提高變得越來越重要。HBM 可以為多種可再生能源工業提供用於結構分析,提高性能的產品,包括核能,風能以及天然氣等。無論是陸地還是海上應用, HBM 都是你理想的合作夥伴.
HBM 產品應用一覽:
Typical applications include:
Measurement data acquisition in high-voltage areas

- Solutions for impulse tests, high-voltage tests.
Tests in high-voltage areas, such as lightning and switching impulse tests place extraordinary demands on the test equipment used. HBM high-voltage products enable reliable measurement data acquisition thanks to electrical isolation, electromagnetic immunity and many other features. The devices have been tried and tested and are used in thousands of applications worldwide. Typical applications include:
- Testing of switching systems, such as switching devices and fuses
- Lightning impulse tests, for example, for testing transformers, surge protectors, isolators and switching systems
- Determination of current zero-crossing.
High-voltage data acquisition solutions
Durability tests on components

- Tests on a blade of a wind turbine with optical strain gauges from HBM
Many structures in the energy industry are subject to high loads: pipelines, power poles or the foundations and towers of wind turbines. Experimental stress analysis is the ideal method to determine stress in materials.
HBM offers a wide range of strain gages and measuring amplifiers as well as professional catman®AP software for experimental stress analysis.
Especially useful for applications in the energy industry: the many possibilities of optical measurement technology using fiber Bragg sensors—measurement with light. Electromagnetic influences can no longer affect the measurement results.
Torque efficiency tests on generators

- T10FH torque transducer from HBM
The demands on the efficiency of generators in all kinds of power plants are increasing dramatically.
Cost pressure and more stringent environmental regulations require knowledge of specific characteristic values reflecting the performance of your generators. HBM is the global market leader in torque measurement—and provides a range of powerful analog and digital torque transducers.
HBM's precise and robust torque transducers are the better choice—in particular in comparison to the indirect torque measurement methods widely used so far.
Weighing technology applications for the energy industry

- HBM weighing module on a gas tank
Whether in gas tanks, with raw materials or in nuclear power plants: Load cells are used in many applications in the energy industry.
HBM's wide range of load cells and weighing indicators offers the right solution for every application—be it for tank weighing or in dynamic weighing processes.
Even in the demanding field of uranium enrichment with high temperature fluctuations, HBM's RTN load cells provide precise and reliable measurement results.
System design, test automation

- HBM nCode fatigue and durability software
Test strain on your systems and structures already in the design phase!
HBM nCode's professional software solutions enable you to carry out "virtual tests" even before starting the production of prototypes. Save costs and increase your efficiency by performing durability and fatigue analyses already in the development phase. Many users from the energy industry, especially from nuclear and wind energy, rely on HBM nCode solutions.
HBM nCode Software Solutions
Wind energy applications
In Wind energy there are versatile applications such as the monitoring of the wind load in the blades of wind turbines in order to increase reliability and availability of wind turbines. The same system can be used to protect the wind turbine from high winds by stopping the machine and turning the blades into a safe position.
Another example for applications in wind energy is power measurement. The mechanical power e.g. of generators needs to be measured accurately with HBM high precision torque transducers according to the standard IEC 60034.
Wind turbine testing with HBM
能源工業的應用報告
World class power testing in ABB's High Power Laboratory
Tests at ABB's High Power Laboratory in Ludvika (Sweden) involve subjecting products to extreme stresses. Advanced test and measuring equipment is used, such as the HBM Genesis HighSpeed measuring system.
GEN2i data acquisition system ensures higher efficiency in generator sets
By utilizing HBM systems, Cummins can now easily meet ABS and ISO requirements while better understanding of performance criteria for its generators.
Chinese develop enhanced diesel engine monitoring system for nuclear power plants
Chinese engineers have developed an engine monitoring system based on HBM’s GEN2i data acquisition equipment to ensure standby diesels meet enhanced nuclear safety regulations.
Long service life and short standstill times with HBM measurement technology
HBM supports highly promising growth markets such as wind energy with state-of-the-art measurement technology. Complete solutions are required to increase the efficiency of wind power plants with HBM measurement technology from...
Isolation improves measurement results
Several factors have an impact on the quality of measurement results. In some applications galvanic isolation is the key to major improvements. This article presents the different topologies and discusses their advantages and...
HBM measurement technology on the test stand: Dynamic torque measurement in water turbines
How can torque be measured more reliably and efficiently? A well-known manufacturer of test stands for water turbines trusts in a new concept: Instead of using a force transducer to measure torque indirectly through the restoring...
HBM technology and service for building up the first German offshore wind farm
Efficiently generating electric power without polluting the environment becomes increasingly important in times of high commodity prices and growing environmental awareness among consumers.
HBM’s nCode Software Selected For Nuclear Reactor Data Analysis
South African based Pebble Bed Modular Reactor (Pty) Ltd (PBMR) has selected HBM’s nCode GlyphWorks and ICE-flow Automation software for the analysis and management of test data.
Measuring chains for biogas installations: RTN load cells for renewable energy sources
There is still no telling where the challenging problem of energy will lead us. We have a maximum of fifty years before fossil fuels become scarce. Which is why new methods of energy production are being called for and developed.
Pictures by Jan Ortgies & Gernot Grundey - Photocase
Solutions for wind turbine testing
HBM offers many professional solutions for tests in the wind energy industry—during the development of plants, but also for structural tests of existing wind turbines.