測量應用報告
測量應用報告 是由獨立撰稿人撰寫的關於測量技術和應用的科技雜誌.
RAM 成立時間是上世紀60年代.
它是由德國 Chemnitz 大學機械學院的 Dr. Martin Stockmann 博士負責編寫的. 每年兩期,有英文和德文版本,並通過 HBM 網站發佈.
Metrological recording of deformation development in ultra-high performance concrete (UHPC) in a triaxial test cell
This article shows that by using a "triaxial cell" test rig, it is possible to determine the triaxial strengths for both static and dynamic loadings.
Numerical simulation of strain gages
This article describes how to apply numerical methods to determine the properties of the strain gages and then, by specifically modifying the material and geometric properties, to change the strain gages so that they meet certain...
Monitoring the Reichenbach and Albrechtsgraben viaducts
Normally, road bridges are visually inspected at regular intervals, in order to detect any defects and/or to decide whether additional rehabilitation might become necessary.
Identifying the material parameters of carbon fiber reinforced plastics with strain gages, taking transverse sensitivity into account
This article describes the process of identifying the material parameters of characteristic carbon fiber reinforced plastics (CRP).
reports in applied measurement
ISSN 1614-9912