Measure high torque with reduced measurement uncertainty
The application of high capacity torque transducers has developed as a result of new international regulations, as well as the need for higher energy efficiency and less fuel consumption.
Apart from the testing of conventional ship combustion engines, the applications for measuring high torque are more or less completely new in the engineering Industry.
Only by integrating torque flanges can a continuous and precise control of ship engines and compressor efficiency be guaranteed – as a result one has significant fuel savings and the ability to fulfil international emission regulations.
HBM is the global market leader for torque flange technology, be it standard or custom transducers, HBM offers significant advantages and solutions in the following applications: