Grid Testing | Switchgear Testing | Solutions | HBM Grid Testing | Switchgear Testing | Solutions | HBM | HBM

Grid Testing Solutions—High Voltage & Switchgear Testing

Grid testing solutions must contend with difficult electromagnetic and environmental conditions, providing clean and reliable measurement results to ensure a reliable supply of power from production through to consumers. Electrical power is—in most cases—not produced where it is consumed. The power grid covers the infrastructure connecting plants with end users, ultimately transporting electrical energy from where it is produced to where it is used.

The power grid is organized into different voltage levels from a few hundred volts (LV), to several 10 kV (MV) up to several 100 kV (HV), depending on the amount of power transportation capacity needed. Thus grid testing products must be capable of handling starkly different voltage levels.

The different voltage levels are interconnected by substations which contain voltage transformers, circuit breakers, surge arrestors, isolators etc. as well as other measurement equipment and switchgear.

Switchgear Tests

Switchgear testing is carried out to ensure reliability and safety of switchgear and circuit breakers. Typical switchgear tests are carried out against applicable standards. They must be carried out in both R&D facilities, for development purposes, as well as at independent test houses, for certification.

Overall grid testing holds a special importance in the economy of a country. So, a strict set of regulations as to how these apparatus should behave and how they need to be tested, has been defined. The “Short-Circuit Testing Liaison (STL)” has created an internationally accepted report called “Harmonization of Data Processing Methods for High Power Laboratories”. This standard describes a set of rules on where and how to measure values in the digitized information.

Read more

HV Impulse Testing

Most of the power grids worldwide are built by power lines on masts. They are highly exposed to lightning strikes with the risk of damage on the components in a substation, which poses a unique problem for grid testing. Damage to one or several of the elements may result in partial loss of the power distribution capability, unsatisfied consumers and high cost for repair. Performing Lightning Impulse testing on transformers, surge arrestors, isolators and switchgear is an important part of the quality proving process and documents the components withstand capabilities.

Read more

Current Zero Testing

Current zero (CZ) refers to the interruption phenomena in high power circuit-breakers. Many, if not all circuit-breakers in commercial use today are working based on contacts moving away from each other, thus creating an electrical arc between the contacts. The current zero phenomena is an indicator for the pressure, temperature, ion density, plasma flow, etc. Current zero measurements are used to understand the phenomena of the arc and to identify the dominant parameters for a successful interruption of the current. This shows the difficulties imposed on grid testing by complex electrical phenomena.

Read more

White Paper: Testing High Power Circuit Breakers Safely

Circuit breakers are ubiquitous wherever there are electrical circuits that need protection against excess current caused by an overload or short circuit. They range in size and capacity from devices the size of a fingernail used for semiconductor protection to devices as large as a truck designed to protect the high voltage circuits that supply power to cities.

Download the full article as pdf