车辆测量 越野设备
结构耐久性 机械工程设备
航空测试 ... 更多!
Somat eDAQ 和 Somat eDAQlite 系统提供给以无与伦比的功能组合:
我们的产品主要用于极端恶劣的环境,并可以现场进行数据处理。这种实时数据处理能力来源于 Somat DataModes™ 技术.
IRT 澳大利亚: SoMat eDAQ 用于澳大利亚铁路轨道运营研究
温度超过 50°C, 灰尘,雨水,震动: 澳大利亚的内陆列车必须在这种恶劣的环境下运行。在设计一种新型的用于铁矿石运输的列车时,全球知名的 轨道技术研究院 (IRT) 决定采用HBM 极为坚固的 SoMat eDAQ 数据采集系统。
Volvo 工程设备
沃尔沃工程机械的测试会持续数分钟到四十五分钟不等,需要对加速度,速度,前后移动,装载和卸载进行各种测试。总共积累的测试数据高达 300 M. 测量数据的分析采用 Infield 软件,在这个阶段,主要是检测数据的质量。 "评估软件对于我们来说非常重要," Lennart Skogh 说 "InField 非常
高速列车测试凸显 HBM eDAQ 数据采集系统优势
用于高速列车,由北京交通大学进行的数据采集系统比较性测试证明了HBM SoMat eDAQ 能够在极端恶劣环境下使用,并能够发挥其所有功能
Gates Corporation
坚固的重新定义: HBM SoMat eDAQ 数据采集系统
The QuantumX MX1615: a Universal Bridge Amplifier
Learn how to make better measurements in the presence of temperature variation, mounting irregularities & electromagnetic interference.
Somat eDAQ Common Field Problems and Solutions
This webinar will explore different workflows for the configuration for large channel count DAQ-systems.
SIMS 专业工程师: 可靠的数据采集确保轨道车辆安全
For a recent series of tests on a new truck trailer design, Sims Professional Engineers (SPE) chose the Somat eDAQ data acquisition system from HBM
How to Setup and Optimize the eDAQ Video Feature
This webinar will demonstrate integrating video into your eDAQ data files. We will review the process of setup, video recording and playback
CAN Based Temperature Data Acquisition with the HBM SoMatCR
This webinar will discuss how to create and load a setup file for the module and show you how to use multiple SomatCR units within a distributed CAN network.
QuantumX Webinar
QuantumX is the world's most innovative data acquisition system. See all benefits at a glance in this recorded webinar session.
Flexible Testing with QuantumX
This webinar will introduce you to QuantumX, a modern distributable DAQ system acquiring all sensor inputs as well as data from various sources.
FFS
法国滑雪联盟 (FFS) optimizes ski cross performance using the HBM measurement chain like strain gages, sensors, SoMat and nCode GlyphWorks.
高速赛车数据采集
Ray Thompson of Thompson Engineering and Racing used the HBM Somat eDAQ-lite to measure the 7 second dragster.
Digital Recorders: the Modern Replacement for your Chart Recorder
This webinar will review the advantages of using a digital data recorder over a paper-based chart recorder.
Increased efficiency in vehicle testing through rugged amplifiers with web interface
In this webinar, we will discuss the requirements of rugged test and measurement equipment and offer you a new convenient solution with a web interface.
Increased Efficiency in Vehicle Testing in Harsh Environments through Web-accessible Data Acquisition
This webinar will explain the requirements needed from rugged test and measurement equipment to ensure reliable data acquisition.
用于车辆现场测试的坚固型数据采集系统
There are different requirements for measurement technology regarding field tests of off-road vehicles. Read here what you need to keep in mind
Testing in real-world conditions: What are the requirements for mobile testing?
This webinar provides you with the basics and everything you need to know on mobile data acquisition.
Somat eDAQ 应用案例: Geisenheim 大学
Geisenheim 大学制定了陡坡机械化种植新概念: 葡萄栽培机器人 "Geisi". Geisi 可以在 70 度陡坡上进行机械化耕种,并可远程控制
Mobile Data Acquisition made Easy
This webinar shows you a robust and clever solution to quickly get results and thus get the most out of your mobile vehicle testing.
Advantages of a distributable and robust DAQ-System for the development of vehicles
In this webinar, we will show you the technical possibilities of mobile DAQ by explaining the example of a crane and a harvester.
step-1: 赛车的测试和测量设备
极速运动与 HBM: step-1 gets open source MiKAR C301B onto the starting line.
Article: How can video support classic sensor data?
HBM survey shows: Recording video data in parallel to tactile sensors or digital bus signals is becoming increasingly attractive to users.