New Printed Circuit Board (PCB) Test Kit New Printed Circuit Board (PCB) Test Kit | HBM

Simplify and accelerate strain measurement on printed circuit boards with HBK’s PCB Test Kit

To help manufacturers avoid damage or failure of their products, HBK has created a Printed Circuit Board (PCB) Test Kit to detect weaknesses during the early stages of development.

Built into many items, such as cars, smart phones and airplanes, PCBs are vulnerable to damage from the mechanical impact and thermal loads they are exposed to during production, transport, and usage over their lifetime. To reduce costs, it is essential the original equipment manufacturers (OEMs) identify root causes of potential failures from occurrences such as deformation, improper use, vibration, shock, or thermal effects. 

As a result, many OEMs or electronic suppliers perform a mechanical load test of the PCBs in compliance with IPC/JEDEC 9704. To simplify testing during R&D or verification in production, HBK created a compact and scalable PCB Test Kit which enables the user to carry out strain measurement tests quickly and obtain accurate results on product reliability.

The PCB Test Kit includes all the necessary material and - in addition to the pre-wired strain gauges and their installation aids - also contains a QuantumX MX1615B bridge module and catman DAQ software. This provides a ready-to-use software project and a pre-configured test certificate report in Microsoft Word format. The PCB Test Kit only accepts commercially available standard products and can be filled up any time. 

The kit includes a one-year software maintenance program and free of charge video tutorials. HBK’s service team is also available for on-site support. 

More information about the PCB Test Kit is available here: www.hbm.com/en/9697/pcb-test-kit

Marketing Coordinator

Heather Wilkins
Telephone: +44 (0) 1223 389 800
Email: [email protected]

Download Press Release

Download Image

About HBK - Hottinger Brüel & Kjaer

For many decades, HBM and Brüel & Kjaer have been trusted across multiple industries to deliver highly accurate technologies and expertise in test and measurement and sound and vibration. HBM as the market leader in testing, measuring and analysis and Brüel & Kjær as the world’s leading solution provider for measuring and managing sound and vibration.

The two companies have now joined forces as HBK - Hottinger, Brüel & Kjaer to form the world’s foremost provider of integrated test, measurement, control, and simulation solutions.

For more information visit www.hbkworld.com