Wie bediene ich ... PMX?
PMX ist das außergewöhnlich präzise, zuverlässige und flexible Messsystem zur Verarbeitung von hohen Datenmengen bei Mehr-Kanalanwendungen. Die folgenden technischen Artikel beschreiben ausführlich, wie PMX in verschiedenen Szenarien betrieben wird.
Hinweis: Die Tech Notes sind in englischer Sprache verfasst.
Wenn Sie Fragen haben, wenden Sie sich gerne an unsere HBM-Support-Mitarbeiter.

Scaling Methods
PMX Adjustment Assistant
This Tech Note gives you an instruction on how to adjust a sensor with the PMX. There are two approaches available to adjust sensors using the PMX: A reference channel from the PMX can be used, or a reference value can be entered manually.
Zum herunterladen jetzt anmeldenPMX Matrix Compensation
This Tech Note will give you an explanation on how to compensate the cross talk of measured values by using matrix compensation. In this example a multicomponent transducer is used, which is able to measure force values within all degrees of freedom.
Zum herunterladen jetzt anmeldenPMX CASMA-Filter
Here you will be given an instruction on how to take the mean of a noisy torque signal with the use of the CASMA-filter (Crank Angle Sampled Moving Average). It works with angular synchronism and is time independent, which makes it able to react to changes of the revolution speed. The PMX provides an own calculated channel for this purpose.
Zum herunterladen jetzt anmeldenFieldbus-Integration
PMX with Siemens PLC and ProfiNet
This Tech Note gives you an instruction on how to create a project with Siemens Tia Portal which connects the PMX to a Siemens PLC. Furthermore, you will be provided with a short explanation on how to monitor measurements from the PMX in Tia Portal. Basic knowledge about ProfiNet connections and the PMX is recommended.
Zum herunterladen jetzt anmeldenPMX with Beckhoff PLC and EtherCat
Here you will be provided with an instruction on how to create a project with TwinCAT which connects the PMX to a Beckhoff PLC. Furthermore, there is a short explanation given on how to monitor measurements from the PMX in TwinCat. Basic knowledge about ProfiNet connections and the PMX is recommended.
Zum herunterladen jetzt anmeldenPMX with Allen-Bradley PLC and Ethernet/IP
This is a guide to creating a project using RSLogix5000 that connects the PMX to an Allen-Bradley controller over Ethernet / IP. Furthermore, there is a short explanation how measured values can be monitored by the PMX in the software. Basic knowledge of Ethernet / IP networking and PMX is recommended.
Zum herunterladen jetzt anmeldenCalculation Channels
Calculating the Force Introduction Point with PMX
This Tech Note will provide you with an instruction on how to determine the force introduction point on a plate with three force transducers.
Zum herunterladen jetzt anmeldenPMX as PID controller
Here you will be given an instruction on how to create a PID controller with the PMX. In this particular example a simple RC circuit first order is controlled. To demonstrate a repetitive process a periodic signal is generate by the internal signal generator of the PMX. This signal is exemplary for any process and can be exchange by other signals (e.g. from sensors).
Zum herunterladen jetzt anmeldenCODESYS-Applications
CODESYS Applications with PMX
This Tech Note provides you with a quickstart guide on starting CODESYS applications for PMX. Basic experience with CODESYS is assumed. Further help is available in the examples that are normally installed on the desktop when the PMX package is imported and in the online Help for the package.
Zum herunterladen jetzt anmeldenCODESYS Application – Data Storage
Here you will be provided with a guide on how to create a CODESYS application on PMX. Basic experience with CODESYS is assumed. Further help is available in the examples that are normally installed on the desktop when the PMX package is imported and in the online Help for the package.
Zum herunterladen jetzt anmelden