Alles, was Sie zur catman-Messtechniksoftware wissen müssen

catman DAQ-Software ist einfach zu bedienen. Um zu erfahren wie einfach sie ist, sehen Sie sich unsere nützlichen Video-Tutorials an, lesen Sie die Tech-Notes und Ihrer Messung steht nichts mehr im Weg.

Video-Tutorials (auf Englisch)

 
Erste Schritte in catman
 
Post-Process: Zyklenzähler
 
Post-Process: Signalgenerator und Playback-Dateien
 
Post-Process: Die Filter im Analysemodus Mode
 
Post-Process: Leistungsspektrum
 
Post-Process: Datensätze
 
Post-Process: Peak-Werte

Anwendungsvideos

Wie Sie einfach Lastdaten ermitteln können und viele weitere Funktionen, wie z-B. die Visualisierung von GPS-Daten in Landkarten sehen Sie in den folgenden Videos.

 
Road Load Data Acquisition with QuantumX and catman
 
General Functions of catman

Tech-Notes Mobile Datenerfassung (pdfs auf Englisch)

The QuantumX Data Recorder CX22-W

This TECH NOTE describes typical application examples of stand-alone data recording using the CX22-W QuantumX data recorder based on catman Easy software and provides tips and hints for optimal parameterization.

QuantumX and SAE J1939 CAN bus

This Tech Note describes how to acquire SAE J1939 CAN signals with QuantumX MX840A or MX471 and the PC software catmanEasy from HBM.

3rd Party Device Integration into catmanAP or QuantumX Data Recorder CX22-W

This Tech Note describes how to integrate a non HBM product / 3rd party device over RS232 into catmanAP and is based on an example using the scripting engine “EasyScript” which is part of the catmanAP package or the Data Recorder CX22 or CX22-W.

Very slow sample rates in catman

The Tech Note describes how to handle very slow sample rates in catman (<1Hz). This is necessary e.g. in monitoring applications.

Integration of Video Signals in catman Easy / AP

This Tech Note describes the related workflow from the configuration of the video cameras to the post processing of the recorded measurement and video data.

catmanAP offline parameterization using Excel Import

This Tech Note describes the workflow to configure the channels of a DAQ system consisting of HBM Quantum X amplifiers and the data acquisition software catman©Easy / AP by using external sensor databases.

Allgemeine Tech-Notes (pdfs auf Englisch)

QuantumX channel Auto Calibration Routine

This TECH NOTE shows in principle the Auto Calibration Routine of analog inputs and how to optimize it.

QuantumX / catmanAP System Diagnosis

This TECH NOTE describes how to get some system information and log files when working with QuantumX and QuantumX Assistant or catmanEASY / AP.


Tech-Notes zu Lab-Tests (pdfs auf Englisch)

QuantumX using Digital Output on Input Channel

This TECH NOTE describes how to use the digital output on QuantumX amplifier MX840, MX440, MX410 or MX460. The amplifiers above offer on pin 15 of the SubHD-15 connector a digital output which can be activated by the PC software level.

QuantumX / catmanAP and Multi IO Module

This Tech Note describes how to parameterize QuantumX digital inputs and outputs of MX879 in catmanAP.

Noise analysis with QuantumX and catman®AP from HBM

This TECH NOTE basically deals with the acquisition and analysis of acoustic signals by means of a measuring microphone, QuantumX measurement electronics, an MX410B amplifier, and catman®AP software.

Digital output signal with catman sequencer and QX MX879

The Tech Note describes how to generate a predefined digital output signal on QuantumX MX879 using Catman-Sequencer.

Passende Produkte

QuantumX: Universelle und verteilbare Datenerfassung
Das perfekte Werkzeug für sämtliche Messungen, Analysen und Tests

Was Sie auch interessieren könnte

Kontakt / Fragen? Wir freuen uns auf Ihre Anfrage.