arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Hoytom, manufacturer of quality control and test equipment, trusts HBK force transducers

Hoytom, Spain

Introduction

Hoytom has always relied on HBK brand products due to the confidence they have in the accuracy and reliability of HBK U10M force transducer.

chevron_left
chevron_right

Hoytom Manufacturer of Test Equipment

Hoytom is a company that specialises in making quality control equipment and electromechanical and electrohydraulic machines for material tests. The capacities of their machines range from 5 kN up to 2000 kN for tensile tests and even more for compression testing.

The Hoytom laboratory has been certified by the ENAC [Spanish National Accreditation Body] since 1996 and provides calibration services on the customer’s premises, issuing the relevant certificates on the condition of their machines, including all areas of force, stress, strain, and hardness. Hoytom’s test machines are the hidden guarantee that ensures that many products on the market meet the function for which they were designed. Test machines are used throughout the manufacturing process of a product − from raw materials to the many intermediate parts that go to make up an assembly.  

Founded in 1961, Hoytom is a Spanish company located in the Basque town of Leioa, near Bilbao, with a staff consisting of experts in the field of static destructive testing, where they stretch or compress devices under test until breakage. Hoytom is a family company going back three generations. Ever since the early days back in the 60s, Hoytom has acknowledged and understood that quality, drive, and the best equipment are key factors to being competitive in the complex world of testing at national and international levels. Testing is as complex as it is surprising.

Anyone who is unfamiliar with testing would be surprised at its size and scope. Everything that reaches the market, the end consumer, industry, construction or most modern businesses, will have undergone some form of test or quality control. Today, it would be unthinkable for a chair to break after a few days of use, or a vehicle component to succumb to physical stress, or a pipe being unable to withstand the internal pressures of the liquid running through it. The guarantee for this not happening is the countless tests performed on materials and components. And these tests and controls are carried out with machines such as those manufactured by Hoytom, and which incorporate top-quality equipment to ensure reliable and accurate results. All this is done in line with the needs of profitability, lead times and other requirements set by the users of these machines. 

INTERNAL USE - Case Study  Hoytom pantalla-mando-1200px
INTERNAL USE - Case Study  Hoytom Hoytom-HBM-1200px

SOLUTION

Hoytom has always demanded top quality load cells for their machines because this is the only way to ensure that the most important aspect of this activity – the data – is totally reliable. Equipping their machines with HBK load cells is a way of offering the very best standards in the sector, that way machines can be sold with a three-year warranty. What’s more, incorporating the HBK brand in their testing machines and hardness testers is an extra marketing tool, as the market values the assurance and quality that this equipment offer.

Anyone who enters this little-known sector soon finds out that testing is a pervasive activity that guarantees the quality of virtually any item in any sector with an incredibly wide range of testing procedures.

Hoytom equipment has always been involved in this field and continues to do so. Hoytom machines have tested many different items – from nuts, bolts and different types of steel, to composites, automotive structures, aircraft parts, cables and concrete. At Hoytom, the managers say they feel most comfortable when dealing with large machines and tests with a certain degree of complexity. Of course, the functionality of the machines is the most important requirement, but for several years now, the company has also offered attractive designs to equip their customers facilities. All this work has come with its own reward: the company now exports 50% of its machines.  

Hoytom’s The testing machines also include hardness testers and pendulums used to determine the hardness and toughness of materials.  

For their universal and hardness testing machines, which carry out Rockwell and Brinell hardness tests, Hoytom has always relied on HBK’s brand products, namely load cells, and integrates them in all their machines, to the point where they have become one of HBK’s main customers in Spain. This is mainly due to the confidence they have in the accuracy and reliability of HBK U10M force transducer, ensuring the minimum values of linearity deviation, hysteresis and reversibility error, together with a high degree of reproducibility. 

RESULTS

The load cells integrated into the Hoytom test machines ensure maximum accuracy throughout the measurement ranges. Combined with Hoytom’s own test control software and with custom-designed electronics, maximum performance, and accuracy are achieved with simple and intuitive use. This level of quality allows Hoytom to enter the international market, to export 50% of their machines and to count on the loyalty of customers that rely not only on the experience and knowledge that Hoytom has to offer, but also on the underlying technology of their machines. 

This commitment increased in 2015, when the current management of Hoytom took over.  Managers were convinced that, in order to improve the machines, one of the key factors was that the load cell and HBK was their first choice. Their previous experience backed up this decision, since HBK had a long history of supplying them with calibration standards and calibration measurement equipment. This allowed working times and disruptions to be reduced, improving the image of Hoytom equipment on the market. It now offers test machines with integrated top-quality cells, which gives customers assurance. All in all, equipping all test machines with HBK U10M was a strategic decision for the company. 

INTERNAL USE - Case Study  Hoytom 2-Hoytom-HBM_1200px
INTERNAL USE - Case Study  Hoytom 1-Hoytom-HBM_1200px
INTERNAL USE - Case Study  Hoytom 3-Hoytom-HBM_1200px

Hoytom test equipment with HBK cells can operate in Class 05 in accordance with the relevant international standard, offering a greater measurement range, a demand that is increasing among companies that conduct tests. But, above all, it is a guarantee of a properly conducted test. In the testing sector, it is essential to invest in top-of-the-range products from a premium brand such as HBK to ensure that reliable data is gathered. And it’s essential to guarantee that the cells will continue to provide reliable data over time, and that corresponding adjustments can be made quickly and easily.   

About Hoytom

Hoytom was founded in 1961 by Don Cipriano del Hoyo and is currently managed by the third generation of the family. The 60's were years that stood out for the weight that the industry began to have in the Basque Country. The new companies saw the need to buy machinery, which used to be acquired in leading European countries such as Germany or even transoceanic countries such as the USA, however foreign trade was not as fluid as it is today.

Technology used

Other case studies

Showing 9 of 511 items
No more result to load