arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

Scansys, Belgium - test rig for dynamic testing of differential gears

Scansys, Belgium

Introduction

Scansys, based in Herstal, Belgium, is a specialist enterprise that develops and produces test rigs for dynamic testing as well as specialist machinery. The main areas of use are pumps, gears, drive units and motors. The customer gets a ready-to-use test rig manufactured to his exact requirements complete with all measurement equipment including that for data acquisition and evaluation. 

chevron_left
chevron_right

For one end customer, ZEXEL of Belgium, the task was to develop high-performance test rigs for dynamic testing of differentials direct in the production line.

The essential requirements of this were:

  • Dynamic torque measurement
  • As accurate as possible measurement of torque and speed of rotation
  • 100% process control in the production line.

In the tendering phase ZEXEL received three quotes, all of which – remarkably – had used the T10F torque flange from HBK for torque measurement.

The deciding factors in Scansys’ choice of torque measuring instrument were the excellent performance and accuracy of the T10F for both dynamic and static applications.

For measurement signal conditioning Scansys uses PME process measurement electronics, also from HBK. As a standard solution the PME system offers a Profibus DP gateway that can be integrated easily into existing process control systems.

Each test rig is equipped with two T10F torque flanges and the relevant PME module MP60-DP. In order to be able to calibrate all the gear test rigs uniformly a DKD-calibrated T10F is used as a reference transducer.

Technology used

No more result to load

Other case studies