Container Reaches its Ideal Weight Thanks to Multi-Trans and HBM
Twenty-four hours. That's how long it takes until a 30-ton container is completely full of slag from a combustion furnace. Then it is replaced by an empty container which can generate some unnecessary costs. Employees have to monitor the filling process to ensure that the container has reached its full capacity. Meanwhile the truck used for the container transport must sit and wait until this is done.
Multi-Trans developed a solution with its custom-made SET 30 electric transporter. The driverless platform trailer replaces the truck that was used during filling for container transport. The innovative transport system also monitors the filling process independently. As a result, there is less use of personnel with no valuable resources tied up– which translates into a considerable boost in efficiency and money saved. Multi-Trans relies on precise weighing technology from HBM for the intelligent platform trailer to perform its tasks. This technology guarantees optimum utilization of loading capacity for the containers that are used, thereby contributing to reliable and independent control of the filling process.



Multi-Trans – individual solutions for internal transport
- Founders: Mathias Floß and Burkhard Pech
- Year founded: 2005
- Number of employees: 20
- Headquarters: Moosburg/Pfrombach
- Products: Heavy-duty trailers up to 150t to customer specification, electric platform trailers, electric tow tractors, gooseneck roll trailers
Multi-Trans GmbH
Naustr. 1
85368 Moosburg/Pfrombach, Germany
Tel.: +49 (0)8762 727923-0
Fax: +49 (0)8762 727923-75
Internet: www.multi-trans.de
E-mail: [email protected]
A driverless platform trailer that thinks
With the self-propelled SET 30 electric transporter, Multi-Trans has created a transport solution that offers users numerous profitable advantages. Not only is the transporter well suited for standard commercial roll containers, its compact dimensions, high loading capacity of 30 metric tons and small turning radius of only nine meters allow for diverse applications. This is accomplished very economically thanks to the integrated weigher which also performs some important monitoring and control tasks.
One example of this is the scenario described at the beginning of this article. First, a truck places an empty roll container on the platform trailer. Then an employee positions the trailer by remote control under a downpipe, where the container receives the slag produced by combustion during the next 24 hours. Once the previously set maximum filling weight is reached, the weighing indicator sends a signal to the conveyor belt and filling stops automatically. An employee is now needed for the first time to guide the weighing platform trailer reliably up to a roll-off tipper, using just a small amount of space. The trailer then automatically receives the roll container from the electric vehicle without the use of any external machines.
HBM turns its expertise in weighing technology to the weighing pan
Using products from HBM, the weigher was integrated into the vehicle and implemented as requested and was completed in a quick and cost-effective manner, while also boosting performance. For example, the HBM 1-RTN/M2LBR22T weighing module is installed by drilling only four holes the size of the modules in the recessed corners of the vehicle. Together with the new 1-RTN0.05/ 15T ring torsion load cell, the new legal for trade WE2111 weighing indicator for industrial applications and the WE2111-ZCC plug-in card from HBM, the weighing module now provides precise and reliable measured values for automatic control of the filling process – which ultimately helps save money.
SET 30 driverless electric transporter
Designation: electric platform trailer
Payload: 30 metric tons max.
Control unit: wireless
Loading area: 6000 x 2600 mm
Steered wheels: all
Drive: an electrically driven axle
Suitable for: roll-off containers up to 6 meters
Special equipment: automatic weight measurement of the load