When developing new products for the oil and gas industry Factory Acceptance Test (FAT) is normally implemented to the life cycle of the new product. The specification is usually created by the end customer through theoretical calculations which needs to be verified and documented. This is then done through tests to make sure the product is ready for installation at the end user´s facilities.
We offer:
- Installation of measurement equipment for these tests.
- Performing measurements, analysis and support on-site.
- The accurate documentation of verification after the tests.
The benefits of hiring our engineers for this job are many. With our expertise we can help you get the tests done in a professional way, provide your customer with the correct documentation in time, thus contribute to future business for you.
See below what one of our oil and gas customers thinks about our services:
"HBM did an excellent job. They were fast, efficient, and even flexible when we needed additional help. We were pleased that HBM could assist us on short notice and help out with analysis and expert assistance during the testing" Gunleik Sandsmark, IRIS’s project manager.