Wärtsilä has developed dual fuel engines that are able to run on either natural gas, marine diesel oil or heavy fuel oil. In order to use the dual fuel engines in marine installations with direct driven propulsion, a precise load signal is required from the engine’s propeller shaft. HBM’s T40MAR torque transducer was accurate enough to offer the data Wärtsilä needed in shipbuilding.
''The main contribution to this remarkable accuracy class is made by the documented unbroken chain of comparisons tracing back the HBM torque transducers to the reference transducer of the German National Standard''
''However, using the dual fuel engines with direct driven propulsion would not be possible without the T40MAR, so we are very pleased with the solution we found together with HBM''Development Engineer at Wärtsilä Marine Solutions, Viktor Häggblom