Manufacturer TECHNOLAS Perfect Vision trusts the reliability of the PMX amplifier from HBM in its devices, as this system consistently provides accurate measured values. Thus every incision of the eye laser is carried out at the exact position and to the correct depth.
The eye operation lasts only a few minutes. The physician does not need to use a blade. The patient can get up shortly after being treated and return home. The patient's visual abilities are restored quickly and without pain. Then the reading glasses can retire to a drawer.
LASIK operations are now performed more than 120,000 times a year in Germany. An excimer laser can be used to treat both nearsightedness and farsightedness as well as corneal curvature and even age-related farsightedness.
The technologies used include the TECHNOLAS® TENEO™ 317 excimer laser and the VICTUS® Femtosecond Laser Platform from manufacturer Technolas Perfect Vision, which belongs to the BAUSCH + LOMB Group.
One special feature of VICTUS® is that the system can be used almost universally. In addition to the wide range of applications for the cornea, cataract operations can also be performed. Ophthalmologists also appreciate the quality with which they can work. All the steps of an operation can be performed perfectly with the laser.