arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management

The Targeted Use of HBM Load Cells in Temo Pese Weighing Solutions

temo pese, Italy

Innovation for Special and Non-Standard Weighing Procedures

Temo Pese has been making industrial scales in Calto (RO) Italy since 1892 and has continued to grow over the years thanks to the company’s passion for its work, which has let it reach and maintain a position of leadership on the mechanical scale market; a position the company consolidated with its electronic weighbridges and other electronic weighing systems. The company’s scales are mainly made of steel or concrete, and it also installs prefabricated weighing platforms in pits.

chevron_left
chevron_right

Innovation, passion, customer relations, professional competence, in-depth knowledge of supply and distribution infrastructures, guaranteed compliance with obligatory and even higher standards: these are the main characteristics of the Italian company from Veneto, focused on continuously innovating and improving its products on the basis of over 120 years of experience in the sector. The fourth generation is currently managing the company and its objective remains the same, to be a reference point in the industrial scale sector, continuing to offer the very best of Italian quality all over the world (in Switzerland, Germany and Slovenia in particular). Synergies with key suppliers play a major role in Temo Pese's business model. Suppliers have been carefully selected over the years for their capacity and ability to offer not only the components they supply, but also their trustworthy advice, technical assistance and co-design. Alberto Bimbatti, the co-owner of Temo Pese, says:

"One concrete example of such synergy is the highly evolved provisioning service provided by HBM, a leading German multinational in the field of measuring systems. We started working with this supplier in 2016, and have had excellent results in the production of a new line of concrete truck scales, which are not very common in Italy but in full expansion in the foreign market."
null

TCA concrete truck scale of highest quality

"The TCA concrete truck scale," continues Bimbatti "was designed and developed to provide a solution of the very highest quality, implementing the advantages of traditional steel weighbridges, including the simplicity of transporting and handling, the flexibility of installation and the limited building work required, with a version made entirely out of reinforced concrete. Pairs of HBM C16 load cells (6, 8 or 10 depending on the truck scale model) are installed to provide the best results for the features and performance required, and to meet our specific needs. The technical service provided by HBM's technicians was essential both when choosing the model of load cell to use and when designing the weighing system, as offering the very highest quality represents a prime objective for both partners." "The C16A column load cells," explains Dario Masato, HBM Italia Sales engineer, "were chosen above all as they’re very strong, precise and reliable, which makes them suitable for any type of application, even the highest level one's, such as Temo truck scale."

nullnullnull

The TCA weighing modules are made of vibrated concrete with the following features:

  • brushed, non-slip surface offering the greatest safety for both vehicles and people in transit when the truck scale is wet, covered with snow or ice;
  • treated with EverCreate Vetrofluid. This is a special waterproofing agent for protecting concrete also in negative pressure up to 10 atm (water column 100 m) that makes it extremely resistant to temperature changes, attacks from chlorides, sulphates and de-icing salts, the formation of mold, algae and moss, as well as preventing reinforcement oxidation;
  • low profile bridge (the angle irons are hot dip galvanized), keeps the amount of building work required to install the weighbridge flush with the pit to a minimum;
  • certified anchor bushings both on the weighing platform and on the profile of the module guarantee the greatest safety also when moving the truck scale in the future.
"We've successfully used the C16 cells in other types of scales, such as modular metal truck scale with three 6x3 m modules, assembled in a framework of eight IPE beams with a longitudinal section of 270 mm. The truck scale framework is covered with 1 cm-thick chequered steel plate. The weight of the modules is supported by brackets welded to the base of each module rather than the two coupling bolts, for greater structural strength. There is a trap door above each load cell for servicing and cleaning. The cables run through fairleads in each module to the junction box. The junction box is mounted on a central module bracket to keep it as dry as possible,"
explains Bimbatti. Prefabricated reinforced concrete flush pit-mounted weighbridges are some of Temo Pese’s top products, and the company from Veneto is the only manufacturer of this type in Italy. These weighbridges can be quickly installed with significant savings in terms of building work costs (the pit can be installed in one day and the truck scale installation takes another day) for a safe and efficient weighing system of highest quality. These prefabricated modules are made of three types of vibrated concrete, which can be combined in a pit wide enough for a 3 m-wide weighbridge of any length:
  • box-section module: two of these modules are used at the ends, where the first pairs of load cells are installed;
  • C module: each of these houses a pair of load cells, and the number depends on the type of truck scale, and as a consequence the number of load cells required;
  • side spacer module: unlike the other two, the length of this module changes depending on the total length of the pit.
null

Related Products

No more result to load