arrow_back_ios

Main Menu

See All Software See All Instruments See All Transducers See All Vibration Testing Equipment See All Electroacoustics See All Acoustic End-of-Line Test Systems See All Academy See All Resource Center See All Applications See All Industries See All Services See All Support See All Our Business See All Our History See All Global Presence
arrow_back_ios

Main Menu

See All Analysis & Simulation Software See All DAQ Software See All Drivers & API See All Utility See All Vibration Control See All High Precision and Calibration Systems See All DAQ Systems See All S&V Hand-held Devices See All Industrial Electronics See All Power Analyzer See All S&V Signal Conditioner See All Acoustic Transducers See All Current and Voltage Sensors See All Displacement Sensors See All Force Sensors See All Load Cells See All Multi Component Sensors See All Pressure Sensors See All Strain Sensors See All Strain Gauges See All Temperature Sensors See All Tilt Sensors See All Torque Sensors See All Vibration See All Accessories for Vibration Testing Equipment See All Vibration Controllers See All Measurement Exciters See All Modal Exciters See All Power Amplifiers See All LDS Shaker Systems See All Test Solutions See All Actuators See All Combustion Engines See All Durability See All eDrive See All Production Testing Sensors See All Transmission & Gearboxes See All Turbo Charger See All Training Courses See All Acoustics See All Asset & Process Monitoring See All Custom Sensors See All Durability & Fatigue See All Electric Power Testing See All NVH See All Reliability See All Vibration See All Weighing See All Automotive & Ground Transportation See All Calibration See All Installation, Maintenance & Repair See All Support Brüel & Kjær See All Release Notes See All Compliance
arrow_back_ios

Main Menu

See All nCode - Durability and Fatigue Analysis See All ReliaSoft - Reliability Analysis and Management See All API See All Experimental Testing See All Electroacoustics See All Noise Source Identification See All Environmental Noise See All Sound Power and Sound Pressure See All Noise Certification See All Industrial Process Control See All Structural Health Monitoring See All Electrical Devices Testing See All Electrical Systems Testing See All Grid Testing See All High-Voltage Testing See All Vibration Testing with Electrodynamic Shakers See All Structural Dynamics See All Machine Analysis and Diagnostics See All Dynamic Weighing See All Vehicle Electrification See All Calibration Services for Transducers See All Calibration Services for Handheld Instruments See All Calibration Services for Instruments & DAQ See All On-Site Calibration See All Resources See All Software License Management
null

The Right Connection

Wiring torque transducers does not have to be difficult. In this article we will show practical tips & tricks on how to connect torque transducers quickly and correctly.

Wiring Universal Torque Transducers

At HBM, we are frequently asked about integrating torque transducers into machinery, and to what extent the onboarding process will affect factory throughput. Different sensors are obviously manufactured to different specifications, with varying electronic and mechanical methodologies. However, modern torque transducers are increasingly designed with ease of integration in mind, to support the demanding measurement requirements of various industrial environments. This article will explore the process of wiring universal torque transducers, such as the T40B, in detail:

Wiring T40B Torque Transducers

 

The T40B is a universal torque transducer for comprehensive bench tests, offering an exceptional 0.03% accuracy in terms of linearity including hysteresis. These transducers are equipped with four electrical ports, which are visibly numbered:

  • Port 1 is a 7-pin plug that provides a voltage supply of up to 30 V to the transducer, and a low resistance path via a shunt. It provides frequency output data;
  • Port 2 is an 8-pin plug with multiple setups depending upon the transducer. It can provide speed measurements and speed with a reference pulse ;
  • Port 3 is another 7-pin plug that is similar to port 1, except it acts as the voltage output;
  • Port 4 is a 16-pin plug that acts as the Torque Measurement Channel (TMC) that can link with interfaces from HBM's TIM family. It provides additional outputs, including scaling, filtering, and zeroes – it can also be connected via CAN or Ethernet-based fieldbuses like PROFINET or EtherCAT for advanced machine-to-machine communication.

These transducers operate on a nominal supply voltage of 18 – 30 V, which is isolated from the signal output pins to reduce background noise. A shunt signal of approximately 50% of the nominal torque signal is generated by T40B torque transducers. As an example, wiring T40B torque transducers with the TIM40 module is simple, and it is easy to test the functionality of the mechanism by observing the LEDs on the stator plate. The TIM40 is easily mounted to mechanical equipment with plainly labeled input and output plugs. Its X1 port is a power supply, while the X2 port is a shunt signal trigger – so it is possible to bypass an external power supply to the transducer by running the TIM40 through the T40B. The X3 plug of the TIM40 is the primary connector to port 4 of the T40B, providing shielding for your torque signal and pass-through power. Finally, the X4 and X5 are frequency and analog outputs, which provide additional limits directly from the TIM40. All the output signals are highly-tunable with good degrees of control, including the naming conventions of signals and the number of decimal points for attained signals.

nullnull

Wiring Torque Transducers with HBM

HBM is a leading developer and supplier of test and measurement equipment, with over 65 years’ experience producing precise instrumentation for test bench systems across the world. We provide full disclosure and thorough documentation to improve integration processes and minimize machinery downtime for customers looking to optimize their test bench systems with minimal installation shortfall. If you would like any more information about wiring torque transducers, please do not hesitate to contact us. Watch our video on wiring torque transducers: 

  • Learn how to wire the torque transducers of type T40B, T12HP and T12
  • General tips & tricks for wiring torque transducers. 

Related Products

No more result to load