New Enhancements to the Genesis HighSpeed Family

Su cuenta en HBM.com

Actualización del registro de usuarios a partir del 17de junio de 2016

***Si ya tiene claves de acceso a HBMshop, puede utilizar la misma información para acceder a HBM.com

The GEN Series product family has several new members: the GEN7i mainframe, the GN815 and GN816 input cards, and the MX1609B temperature module. This webinar will review the features and benefits of each product with an emphasis on new capabilities. These new members of the Genesis HighSpeed product family make it easier than ever for you to work more efficiently and get even more accurate and reliable results.

Contáctenos Contacte con HBM si desea saber más sobre lo que HBM le puede ofrecer.