Webinar: Power measurement on wind turbine generators

Su cuenta en HBM.com

Actualización del registro de usuarios a partir del 17de junio de 2016

***Si ya tiene claves de acceso a HBMshop, puede utilizar la misma información para acceder a HBM.com

Please login to access the recording.

High energy conversion efficiency is crucial for efficient operation of wind turbines. Efficiency is the ratio between the generators' power output and the power consumed. Analyzing the resulting stored raw data provides insights into how the generator's efficiency can be increased. However, this requires adequate test and measurement equipment.

This webinar explores how to determine and increase efficiency through

  • Determination of the generators' mechanical input power using torque transducers
  • Determination of the generators' electrical output power using the Genesis HighSpeed data acquisition system
  • Analysis of resulting raw data

Speakers:

Klaus Lang

Focus Sales Manager Test and Measurement at HBM

Contact:

[email protected]

 

Dr. André Schäfer

Product and Application Manager Wind Energy at HBM Test & Measurement

Contact:

[email protected]

Contáctenos Contacte con HBM si desea saber más sobre lo que HBM le puede ofrecer.