Structural Testing (Application)

Webinar: Strain gauge specifications: What do I need to know and take into account when taking measurements? - February 22, 2017
In this webinar, you’ll learn how to correctly interpret the properties of strain gauges and what specifications you need to pay special attention to in your application.

Webinar: Multi-channel data acquisition with high sample rate requirements – How to solve the challenge of high data throughput
The webinar will explain the usage of a modular and scalable data acquisition system for fast measurements of electrical and mechanical quantities. You will learn how to use a modern data acquisition system as a transient recorder and data recorder at the same time.

Webinar: Load Data Acquisition in Harsh Environments
Load data acquisition of machines and vehicles in the field can be tough: The webinar explains how to integrate digital signals like video cameras, GPS and field busses in addition to analog sensor signals in harsh environments.

Residual Stress Analysis Using the Hole Drilling Method
This webinar presents the hole drilling method for residual stress analysis using the high speed drilling method.

Protecting Strain Gauge Measuring Points - Tips & Tricks
Learn which covering materials are available and how to select the appropriate covering agent in this webinar.

Understanding the Wheatstone Bridge
The resistance change of strain gauges is usually measured using Wheatstone bridge configurations. The webinar will show what to consider for trustworthy measurements and which pitfalls to avoid.

Assess and minimize measurement uncertainty for strain gauge measurements
What are the influence quantities that determine the accuracy of a strain gauge measurement? Our webinar will provide the answers.

FACC: Testing the winglets of the Airbus A350XWB with HBM Strain Gauges
Strain gauges from HBM helped to measure results of the static and fatigue tests on winglets of the Airbus A350 XWB.

How to Reduce Measurement Uncertainty Throughout the Entire Force Measurement Chain
The webinar will explain the main aspects of measurement uncertainty along the complete force measurement chain – from real sensor to digital data stream.

Temperature Compensation of Strain Gauges
This webinar describes the influence of temperature on strain gauge measurements and the available solutions to avoid measurement errors.

Fatigue and Durability Testing
The webinar describes the laboratory tests commonly used to determine the fatigue life of materials and structures for lightweight construction of vehicles, machinery and components.

Quality testing of a pipe for the oil industry (IRIS Institute)
HBM supported IRIS institute in Norway to take measurements using strain gauges and a data logging system to prevent delays in the work of a new pipeline model.

Strain measurements play key role when Bromma develops new lifting beam
As part of their product development, Bromma wanted to verify its theoretic models by measuring tension in the steel used for lifting beams.

Tips for experimental stress analysis
Our series of articles addresses possible sources of error when strain gauges are used in experimental stress analysis and shows how to successfully assess measurement uncertainty already in the design stage.

Temperature Compensation of Strain Gauges
This webinar describes the influence of temperature on strain gauge measurements and the available solutions to avoid measurement errors.

Optical and electrical test and measuring equipment in structural analysis
In this webinar, we will provide you with detailed information about hybrid measuring chains and, in particular, about the interface between the data acquisition system and the software

Selecting the Right Strain Gauge, Adhesive and Covering
This webinar will discuss key elements to consider when selecting strain gauges, adhesives and coverings for your applications.

Hole Drilling Residual Stress Measurements with the MTS3000
The MTS3000 is a complete solution for measuring residual stress when employing the hole-drilling strain-gauge method, in accordance with ASTM standard E837-13. The test can be automated, thus ensuring high accuracy and repeatability of the measurement.

How to get the most out of your optical interrogator
In this HBM webinar, the Smart Peak Detection (SPD) method that allows the accurate detection of all sensors in large optical networks is explained.

Durability Testing On High Tensile Materials
In this webinar we will discuss the displacement of an S-N curve using a new HBM product as an example.

Hole-drilling residual stress measurements with the MTS3000: complete system setup, connection and test
This webinar shows all the main steps for preparing and performing a correct measurement.

Measurements at high strain levels
Measurements at high strain levels – New series of electrical strain gauges with increased resistance to alternating loads

Optical Fiber Sensors Unveiled – How These Sensors Will Fulfill your Application Needs (US)
In this webinar, you will be guided through the fundamental concepts of optical fiber technology and how it can be used for sensing.

Optical fiber sensors unveiled – How your needs can be fulfilled
In this webinar you will be guided through the fundamental concepts of optical fiber technology and how it can be used for sensing.

Residual stress measurements by hole drilling in accordance with ASTM E8372013
In this webinar, you will learn more about the EVAL software upgrade in accordance with the new version of the ASTM E837 standard.

Mechanical Stress Testing of Materials Validates Finite Element Analysis
This webinar focuses on mechanical stress testing of elastic materials. The data is used to validate FEA models for material development and testing.

Residual stress analysis using the hole drilling method
This webinar presents the hole drilling method for residual stress analysis using the high speed drilling method.

How to calculate a strain gauge's excitation voltage
Compliance with a strain gauge's maximum permissible bridge excitation voltage is essential to avoid measurement errors. This webinar explains what this value means and how it is calculated.

Strain Gauge Excitation
The maximum effective bridge excitation voltage is an important parameter in the technical data sheet of a strain gauge. This webinar will examine bridge excitation voltage in detail.

Critical Elements to Consider in Choosing Strain Gages for Sensor Design
Webinar about critical elements to consider in choosing strain gauges by Randy Hopkins, Sensor Business Director at HBM, Inc.

From Strain to Report Using Strain Gages to do Experimental Stress Analysis
This webinar is about selecting a strain gauge, connecting the strain gauge (2, 3 or 4 wire), setting up an amplifier and the software.

BAE Systems
BAE Systems benefits the performance of the new F-35 Joint Strike Fighter through integrated structural testing and derisking the FTI.

MGCplus - The renowned scalable and configurable data acquisition system for laboratory and test stand
The ultimate, scalable and configurable data acquisition system, for laboratory and test stand use, achieving acceptance as a measurement standard.

Mechanical Component Testing

How to Reduce Measurement Uncertainty Throughout the Entire Force Measurement Chain
The webinar will explain the main aspects of measurement uncertainty along the complete force measurement chain – from real sensor to digital data stream.

Selecting The Right Filter for Your Application

Selecting the Right Amplifier for Your Application
In this webinar you will learn when it is necessary to use isolated amplifiers as well as the differences between balanced versus unbalanced, symmetrical versus unsymmetrical and differential versus single-ended amplifiers.

High-speed Data Acquisition in Strain Measurement and Dynamic Material Testing Applications
This webinar will give an introduction to high-speed data acquisition in strain measurement. View this webinar today.

Enhancements to the Genesis HighSpeed Family
The GEN Series product family has several new members: the GEN7i mainframe, the GN815 and GN816 input cards, and the MX1609B temperature module.

PCB Testing
This webinar will discuss the problems you may encounter while stress testing PCBs and how to solve them.

Strain Gauge Measurements on PCBs
This webinar will discuss the problems you may encounter while stress testing PCBs and how to solve them.

Using LabView with HBM DAQ
Several of HBM’s data acquisition systems provide easy-to-use interfaces when used with the LabVIEW software.

Configuring an Amplifier for Data Acquisition
Watch the recording of the HBM online webinar on how to configure an amplifier for professional data acquisition.

Infield’s Test Control Module
This webinar will examine the many uses of Infield’s Test Control Module(TCM) such as data acquisition, visualizing live test run data and statistical data, and setting up post run statistical and time history outputs.

CANape with HBM High Speed DAQ
Webinar on how to integrate ECU internal signals in your measurement as well as how to integrate QuantumX data acquisition in the CANape software.

Acquiring and Interpreting CAN message data with Somat eDAQ hardware
This webinar will provide a brief overview of the CAN communication protocol. We will look at how the Somat eDAQ can be used to record and interpret CAN message data.

Selecting the right filter for your application
This webinar will share information about the new features in Perception 6.30, and the long anticipated 1kV DAQ module for HBM's GEN series.

catman’s Transducer Database
HBM catman Easy’s sensor database will help you save test setup time and money. This webinar will show you how your commonly used sensor settings can be stored in the database and assigned to your test with a click of a mouse.

LISA Airplanes
Making flying a pleasure again: This is the aim of the new, ultra-modern AKOYA light airplane through the use of strain gauges from HBM and the ultra-rugged SoMat eDAQlite data acquisition system.

ORWIN
Orwin, one of largest automation machine builders in the UK, has utilised HBM’s MP85ADP amplifier in an Active Engine Mount Cell assembly line.

MGCplus - The renowned scalable and configurable data acquisition system for laboratory and test stand
The ultimate, scalable and configurable data acquisition system, for laboratory and test stand use, achieving acceptance as a measurement standard.

Powertrain Testing

T40FH Torque Sensor For Extremly High Torque (up to 300 kN·m)
The T40FH digital torque flange for high torque up to 300 kN·m

Using the CASMA Filter for Torque Measurements - Tips & Tricks
In this article you will learn how to apply the CASMA filter in HBM's TIM-PN, TIM-EC and PMX signal conditioning systems.

Efficiently Measuring Torque in Marine Applications
Learn how strain links and electronics can help you optimize your measurement in a press or similar application.

T40MAR certified transducer for determining the load signal
T40MAR is the torque transducer for reliable acquisition and control of the load signal on ships.

How to Select a Rotating Torque Sensor
Learn how to perform measurement-centric control and data management for process monitoring, condition monitoring and end of line testing on industrial test rigs.

Mahle Powertrain: HBM helps make engines go greener
Mahle Powertrain: HBM helps make engines go greener

T40B Universal Torque Transducer for Test Benches
The T40B torque sensor is ideally suited for test bench applications , as well as End-of-Line tests.

INVT
The company INVT has utilized HBM’s T10F torque transducer to measure torque and speed of an electric motor in order to optimize performance.

T40FM Torque Transducer for Dynamic Torque Measurement
The T40FM torque transducer measures dynamic torques up to 80 kN·m precisely and reliably.

T10F: Tried and Tested Torque Flange for Many Applications
The T10F torque transducer is well proven and reliable and can be used in many applications.

T12 Torque Transducer offers maximum precision
Precise digital torque transducer for use in modern test benches and industrial applications

MGCplus - The renowned scalable and configurable data acquisition system for laboratory and test stand
The ultimate, scalable and configurable data acquisition system, for laboratory and test stand use, achieving acceptance as a measurement standard.

Mobile Data Acquisition

Advantages of a distributable and robust DAQ-System for the development of vehicles
For the testing and inspection of vehicles, mobile data acquisition is certainly the hardest and most interesting of all challenges. In our webinar, we will show you the technical possibilities by explaining the example of a crane and a harvester.

Mobile Data Acquisition made Easy
You want to get the most out of your mobile vehicle test? This webinar shows you a robust and clever solution to quickly get results and thus get the most out of your testing.

Somat eDAQ Case Study: University of Geisenheim
Geisenheim University has developed a new concept for mechanized work on steep slopes: the viticulture robot "Geisi". Geisi shall have the capability to work on slopes of up to 70 percent - remote controlled and without ropes.

Testing in real-world conditions: What are the requirements for mobile testing?
This webinar provides you with the basics and everything you need to know on mobile data acquisition.

Rugged data acquisition systems for field tests of off-road vehicles
There are different requirements for measurement technology regarding field tests of off-road vehicles. Read here what you need to keep in mind.

Increased Efficiency in Vehicle Testing in Harsh Environments through Web-accessible Data Acquisition
This webinar will explain the requirements needed from rugged test and measurement equipment to ensure reliable data acquisition.

Increased efficiency in vehicle testing through rugged amplifiers with web interface
In this webinar, we will discuss the requirements of rugged test and measurement equipment more in detail and offer you a new convenient solution: A flexible and very rugged DAQ system with web interface.

Digital Recorders: the Modern Replacement for your Chart Recorder
This webinar will review the advantages of using a digital data recorder over a paper-based chart recorder.

Thompson Engineering and Racing
Ray Thompson of Thompson Engineering and Racing used the HBM Somat eDAQ-lite to measure the 7 second dragster.

FFS
French Skiing Federation (FFS) optimizes ski cross performance using the HBM measurement chain like strain gages, sensors, SoMat and nCode GlyphWorks.

Flexible Testing with QuantumX
This webinar will introduce you to QuantumX, a modern distributable DAQ system acquiring all sensor inputs as well as data from various sources.

QuantumX Webinar
QuantumX is the world's most innovative data acquisition system. See all benefits at a glance in this recorded webinar session.

Acquiring Reliable Data Quickly and Easily with High Accuracy DAQ
In this presentation, learn how HBM’s most accurate tools can help you save development time and effort over traditional methods, reduce system cost, produce high quality, repeatable data and cut your project timeframe by up to 10X.

CAN Based Temperature Data Acquisition with the HBM SoMatCR
This webinar will discuss how to create and load a setup file for the module as well as show you how to use multiple SomatCR units within a distributed CAN network.

How to Setup and Optimize the eDAQ Video Feature
Ever run a test and wondered what caused the data anomaly in the middle of the test? Integrate Somat eDAQ video into your test, to answer those questions.

SIMS Professional Engineers: Reliable Data Acquisition Ensures Rail Car Safety
For a recent series of tests on a new truck trailer design, Sims Professional Engineers (SPE) chose the Somat eDAQ data acquisition system from HBM.

Somat eDAQ Common Field Problems and Solutions
This webinar will explore different workflows for the configuration for large channel count DAQ-systems.

The QuantumX MX1615: a Universal Bridge Amplifier
Learn how to make better measurements in the presence of temperature variation, mounting irregularities & electromagnetic interference.

Gates Corporation
Redefining Rugged: HBM’s SoMat eDAQ Data Acquisition System

Chinese tests highlight superiority of HBM’s eDAQ solutions
Comparative tests of data acquisition equipment for use on high-speed trains undertaken by the Beijing Jiaotong University in China have demonstrated the effectiveness of HBM’s SoMat eDAQ equipment when operating under extremely tough conditions

Volvo Construction Equipment (CE)
Volvo Construction Equipment uses HBM's SoMat eDAQ test system to help it test loader prototypes under extreme conditions.

IRT Australia: SoMat eDAQ used in Australian rail operations tests
The Institute for Rail Technology decided to use HBM's SoMat eDAQ data acquisition system when designing a new measurement vehicle.

C18
For stationary and mobile use. Insensitive to humidity effects and rugged cable routing.

P8AP
Absolute pressure transducers of the P8AP type series are suitable for measuring static and dynamic liquid and gas pressures.

RTN
Ideal for platform scales, truck scales, and tank weighing, the RTN Ring Torsion Load Cell from HBM covers a large rated load range from 1t to 470t.

eDrive Testing

768 KB 487 KB 3 MB

eDrive Testing - Better Results Lead to Increased Efficiency
Data acqusition and analysis at inverter driven electrical machines from power and efficiency measurement to accelerated motor mapping.

Power measurement on wind turbine generators
This webinar explores how to determine and increase efficiency of wind turbine generators

Integrated test and measurement equipment for electric motors and inverters
In this webinar we explain what, from the test and measurement point of view, is key to testing electric motors and inverters in the electric drive train.

T40FM Torque Transducer for Dynamic Torque Measurement
The T40FM torque transducer measures dynamic torques up to 80 kN·m precisely and reliably.

Advanced measurements and analysis at variable frequency electric drives
In this webinar we present an integrated measurement solution for inverter driven electrical machines.

T10F: Tried and Tested Torque Flange for Many Applications
The T10F torque transducer is well proven and reliable and can be used in many applications.

2 MB

T40B Universal Torque Transducer for Test Benches
The T40B torque sensor is ideally suited for test bench applications , as well as End-of-Line tests.

T40HS – For high-speed torque applications above 45,000 rpm
T40HS is the space and cost saving torque transducer for your high-speed application above 45,000 rpm, characterized by its short design, its high stiffness and its outstanding precision.

Webinar: Accelerated efficiency mapping of electric machines with 3 or more phases - April 25, 2017
In this webinar you will learn how to significantly accelerate the process of generating an efficiency map for an electrical machine with the help of HBM’s eDrive solution.

T12 Torque Transducer offers maximum precision
Precise digital torque transducer for use in modern test benches and industrial applications

Measuring temperatures and voltages on high electrical potential
Do you want to measure temperatures at a high electric potential - very precisely and, above all, reliably? The webinar presents all the aspects of a complete solution that enables temperatures as well as voltages and currents to be precisely and, above all, reliably measured and analyzed.

White Paper: Efficiency and Loss Mapping of AC Motors
This article describes an accelerated process to create motor maps in a few minutes only and then describes the analyses of the data to create efficiency and loss map, and MTPA trajectories.

Article: Test and Measuring Equipment for Hybrid Test Benches
Drive hybridization means that requirements for test bench test and measuring equipment have become considerably more stringent. HBM's eDrive solution offers turnkey test and measuring equipment for even the most complex test benches, including real-time transfer of data to the automation system.

Motor and Inverter Testing on Electrical Drive Trains
Measure the efficiency of electrical motors, inverters and the entire electric drive train to improve the range of electric automobiles and the efficiency of aircraft power systems during dynamic load changes.

Efficiency Testing on Electrical Drive Trains
What is key to testing electric motors and inverters in the electric drive train. The focus of attention is on optimizing the efficiency measurement through continuous and synchronized acquisition of the electrical and mechanical power.

Efficiency Testing on Electrical Drive Trains (US)
What is key to testing electric motors and inverters in the electric drive train. The focus of attention is on optimizing the efficiency measurement through continuous and synchronized acquisition of the electrical and mechanical power.

GREENMOT
HBM, a key partner for the french company Greenmot, provides DAQ systems for testing.

Bertrandt
More efficient electric motors through accurate analysis of the drive using raw data

eDrive testing - Brochure

2 MB 2 MB

eDrive testing - Brochure

2 MB

eDrive testing - Brochure

2 MB

eDrive testing - Brochure

2 MB

Power Analyzer Alternative
When testing electric machines, a power analyzer is like having a good set of cards. But choosing a GEN3i is like having a royal straight flush!

Power measurements on a pulse width modulated inverter with Perception software
The development of electric drives requires power measurements at inverters. This article describes the calculation of pwer quantities using Perception software.

Calculation and realization of measured quantities in electrical energy technology as space vectors with HBM Perception software
The article describes how to convert measured 3-phase current and voltage quantities into space vectors and dq0-components using Perception software.

Dynamic Testing and Analysis of Inverters, Electric Motors and Generators Beyond the Typical Power Analyzer
Learn about a unique testing solution that allows engineers to continuously study both electrical and mechanical performance and efficiency parameters

How Torque Transducers Help Optimize Hybrid Drivetrains for Buses and Trucks
HBM Torque transducers helped on customers optimize hybrid drivetrains by gathering data engineers would not typically see.

Dynosens
Dynosens needed an interface to connect its T40B torque transducer to the EtherCAT fieldbus. The solution: TIM-EC from HBM.

What drives electrical machines and inverters: More efficient analysis with eDrive Testing by HBM
HBM’s innovative eDrive Testing solution makes it possible to record mechanical and electrical signals synchronously and dynamically.

Parameterization of an incremental rotary encoder
How an incremental rotary encoder - already connected to an electrical machine - can be analyzed by a Genesis data recorder.

Seven misconceptions about the testing of electric motors
We reveal to you the seven major misconceptions about eDrive testing - and how you can enhance your testing of electric motors.

INVT
The company INVT has utilized HBM’s T10F torque transducer to measure torque and speed of an electric motor in order to optimize performance.

Test Rig for Induction Motor Quasi-Static Electromechanical Characteristic Determination
This article presents a test rig for the determination of the quasi-static electromechanical characteristics of induction motors.

Switchgear Testing

Power Testing in the ABB High Power Laboratory
Tests at ABB's High Power Laboratory in Ludvika (Sweden) involve subjecting products to extreme stresses. Advanced test equipment from HBM is used.

Electrical Grid Testing Aircraf

Advanced aircraft electric system testing
This webinar explains HBM’s solution for advanced testing of components and the complete electrical grid of an aircraft.

Advanced Aircraft Electric System & Equipment Testing
One universal DAQ system for the electrical, mechanical and efficiency testing of all components of the aircraft electric system testing.

QuantumX CX22B-W Data Recorder
Data recorder QuantumX CX22B-W collects, analyzes and stores acquired measurement data directly in the device - without any PC connection

CLES-FACIL
The Task of the 2011 experimental rocket was to fine out the force that the openings of a parachute exerts on a rocket.

BAE Systems
BAE Systems benefits the performance of the new F-35 Joint Strike Fighter through integrated structural testing and derisking the FTI.

Shock Tests

Increased efficiency in vehicle testing through rugged amplifiers with web interface
In this webinar, we will discuss the requirements of rugged test and measurement equipment more in detail and offer you a new convenient solution: A flexible and very rugged DAQ system with web interface.

Shock, Vibration and Impact Testing with Genesis High Speed
Genesis High Speed DAQ system provides absolute data security, plus an extremely high sample rate of up to 100 MS/s for shock, vibration and impact tests.

POLITECNICO DI MILANO
Italian researchers have selected HBM’s GEN7t high-speed equipment to improve the reliability and accuracy of data acquisition on Charpy tests.

CLES-FACIL
The Task of the 2011 experimental rocket was to fine out the force that the openings of a parachute exerts on a rocket.

Durability Tests

From Strain to Report Using Strain Gages to do Experimental Stress Analysis
This webinar is about selecting a strain gauge, connecting the strain gauge (2, 3 or 4 wire), setting up an amplifier and the software.

Residual Stress Analysis Using the Hole Drilling Method
This webinar presents the hole drilling method for residual stress analysis using the high speed drilling method.

Hole Drilling Residual Stress Measurements with the MTS3000
The MTS3000 is a complete solution for measuring residual stress when employing the hole-drilling strain-gauge method, in accordance with ASTM standard E837-13. The test can be automated, thus ensuring high accuracy and repeatability of the measurement.

CRH
C. Rob. Hammerstein (CRH), globally leading manufacturer of car seats, has developed a future-proof test concept, trusting in measurement technology from HBM.

Industrial Measurements (IPC)

SLB700A/06VA
Active strain transducer with voltage or current output. Enabling in particular large forces to be measured in a cost efficient way.

Reduce Your Effort! Update Your Test Cells, Systems and Monitoring without Software Programming
In this presentation, learn how to add new signal conditioning capability, channels and real-time decision making to your existing test and monitoring systems without changing the already developed software.

Force measurement using strain transducers
In this webinar, we would like to present strain sensors and amplifiers that are suited to force measurement. Using the example of the SLB700A strain sensor and the PMX measuring amplifier we will explain the requirements to be met when measuring with these sensors. In addition, we will demonstrate how to calibrate such a measuring chain in just a few steps.

5 decision-making criteria for selecting your industrial amplifier
The use of amplifiers in production is an essential part of your quality assurance process. What are the decision-making criteria you should take into account when selecting a new industrial amplifier?

Webinar: Test bench and control technology with intelligent automation systems - February 23, 2017
The presentation shows what modern Automation-systems must offer today: precision & robust measurement technology, control and monitoring functions in real-time and easy operation without special programming knowledge - and how this is easy and inexpensive to reach times of industry 4.0.

P3IC / P3ICP Industrial Class
High-quality series P3IC "Industrial Class" pressure tranducers from corrosion-resistant steel are specially suited to use in industrial applications

P2VA1 / P2VA2
Used for the precise analysis of production processes, as well as for fast control loops, where even short pressure peaks are reliably mapped.

P3 Top Class BlueLine
Highest pressures ranging between 5,000 and 15,000 bar need to be measured in an increasing number of industrial applications

T5 Slip Ring Torque Transducer Shaft Design
Torque flange designed for occasional, simple torque measurement tasks in the laboratory, teaching and testing sector.

T4A Slip Ring Torque Transducer Square Shaft Design
Specifically designed for measuring static and dynamic torque, rotation speed and angle of rotation in production monitoring and quality assurance.

T22 Cost Effective Torque Transducer for Standard Industrial Applications
Cost effective transducer for standard industrial applications. Acquires torque using strain gages and contact-less energy and signal transmission.

T20WN Torque Meter with Cylindrical Shaft Stubs
Specifically designed for measuring static and dynamic torque, rotation speed and angle of rotation, the HBM T20WN torque transducer.

KMR
Rugged transducer offering high degree of protection for use in harsh ambient conditions

U93
High lateral force stability, practice-oriented configuration (connectors, cable lengths, TEDS)

T12 Torque Transducer offers maximum precision
Precise digital torque transducer for use in modern test benches and industrial applications

NIST
Researchers in the USA have utilized HBM’s DAQ equipment to ensure international competitiveness, to improve the quality of their products.

Load Monitoring Systems in Press Applications
Learn how modern sensors and electronics like strain gages can help you optimize your measurement in a press or similar application.

Article: Industrial Internet of Things
HBM White Paper - Innovative metrological solutions for the challenges of modern, networked production systems (IIoT)

Dynamometer Engine Testing
Learn how to perform measurement-centric control and data management for process monitoring, condition monitoring and end of line testing on industrial test rigs.

Optical and Electrical Test and Measurement in Structural Monitoring
In a live presentation we will show you a new function of our catman measurement software that allows integration of optical interrogators from HBM FiberSensing.

Integration of PMX with Torque Transducers at BCSA
Case Study about an innovative application by the French company BCSA that uses HBM technology.

Measure, Control and Connect with PMX
Learn how to perform measurement-centric control and data management for process monitoring, condition monitoring and end of line testing on industrial test rigs.

Measurement uncertainty force transducers
In this HBM webinar you will learn what factors impact measurement uncertainty in force measurement chains.

Efficient control solutions in mechatronic systems
This HBM webinar introduces new possibilities for making control solutions in mechatronic systems more efficient.

Get the most out of TEDS (Transducer Electronic Data Sheet)
Learn how the TEDS technology makes the setup of a measurement chain reliable and fast in this webinar.

Ketten Wälder
Quality assurance is essential for producing chains for hoisting gear, Ketten Wälder GmbH uses HBM measurement technology in its production systems.

Ethernet in production areas
Ethernet is increasingly more popular in the industrial environment, why is this and is Ethernet suitable for the high requirements in production?

Rapid measurement data acquisition for industrial applications
Due to increasingly demanding requirements in industrial measurement data acquisition HBM is introducing PMX the new industry standard for measurement

Modularity and modern operating concepts for industrial measurement technology
Modularity and modern operating concepts for industrial measurement technology. The new PMX system offers significant advantages in this field

DD1
The basic unit is a displacement transducer which converts the movement of a probe tip into an electrical signal.

SLB700A
Strain transducer for force measurement; is simply bolted onto the structure. Also available as a transducer with integrated amplifier. Current or voltage output.

Integration of Torque Sensors into Automation Environments using TIM-EC
The TIM-EC interface module enables torque sensors to be easily integrated into automation environments, providing users many benefits.

PMX - control system combines high-quality measuring and testing technology in mechatronic systems
Read in this article from HBM and learn more about the requirements for mechatronic systems and the applied smart measurement technology.

Torque Flanges in power generation plants
As the biggest manufacturer worldwide of torque flanges for torque measurements, HBM has decades of experience in this sector.

EoL Production Tests

Ketten Wälder
Quality assurance is essential for producing chains for hoisting gear, Ketten Wälder GmbH uses HBM measurement technology in its production systems.

End of line Powertrain

Filling, Sorting, Checkweighing

WTX120: Industrial and Legal for Trade Weighing Terminal
The rail-mountable and easy-to-use WTX120 industrial weight indicator offers PROFINET, EtherNet/IP and PROFIBUS interfaces. Connect any analog load cell.

BLC: Legal for Trade Load Cell with Maximum Capacities from 550 kg up to 1.76 t
Load cell with maximum capacities from 550kg up to 1.76t, and an accuracy class of D1 and C2 (OIML). Fit for use in many different applications.

PW25 Easy-care load cell for high hygienic standards
The PW25 load cell is highly precise, very rugged and easy to clean. That makes it ideally suited for use in the food industry.

How digital weighing technology saves you money
In this webinar, several application examples will demonstrate how you can save money with digital load cells thanks to their new functionalities.

S+P Wägetechnik GmbH
New mobile wireless scales by S+P remain operational for 4 weeks without recharging. This is due to the know-how and experience of HBM.

Article: Digital Weighing Technology in the Food Industry
Digital strain gauge based load cells ensure greater productivity for almost any application in the food industry than load cells based on electromagnetic force compensation (EFC).

Tropper
On board weighing: TROPPER using RTN load cells for the highest level of reliability

Cemex
In order to ensure optimal mixing and dosing of the material anhydrite flow, CEMEX Austria is using HBM weighing technology.

PW15PH Hermetically Encapsulated Single Point Load Cell
The hermetically encapsulated PW15PH single point load cell is made of stainless steel and has a unique connector system.

PW27 Aseptic Load Cell
The PW27 aseptic load cell was developed especially for the food industry. It is particularly easy to clean and certified by the European Hygienic Engineering & Design Group (EHEDG).

New sensor concepts for checkweighers

Fine-Spect
The French company Fine-Spect has developed a new checkweigher. The core element of the new checkweigher is the strain gauge-based FIT7A digital load cell from HBM.

ALL FILL
All Fill International has a long history of working with HBM and has used both its digital and analogue models. This includes using HBM’s FIT1 digital load cells.

FIT7A Video Tutorial: Setting up a checkweigher
This video demonstrates how you get quick and precise results using the FIT7A digital load cell and the PanelX software by HBM.

Straightpoint
British load-testing specialist Straightpoint uses HBM strain gauges in all of its force measurement, load monitoring and load cell products.

Process & Level Monitoring

Wägezellen in explosionsgefährdeten Bereichen

WTX120: Industrial and Legal for Trade Weighing Terminal
The rail-mountable and easy-to-use WTX120 industrial weight indicator offers PROFINET, EtherNet/IP and PROFIBUS interfaces. Connect any analog load cell.

Advantages of digital weighing technology
This webinar offers an initial overview of the advantages of digital weighing technology in comparison with traditional analog systems. You will furthermore see, how you can save development time with modular digital weighing concepts.

Scale Manufacturing

WTX120: Industrial and Legal for Trade Weighing Terminal
The rail-mountable and easy-to-use WTX120 industrial weight indicator offers PROFINET, EtherNet/IP and PROFIBUS interfaces. Connect any analog load cell.

More efficient ordering, easier configuration: Tips and tricks for using the HBM online shop
More and more HBM customers order from our new online shop - a convenient and modern way to purchase your test and measurement components. However, the HBMshop offers more: It is a complete customer platform for you. In this webinar we show you how to benefit from the online shop - and what useful features are provided.

New sensor concepts for checkweighers

Requirements for medical lifter scales: quality and safety
Requirements for medical products are high and the same applies to lifter scales. Quality assurance and traceability play a major role.

New Healthtech range features HBM's load cells
The UK scale manufacturer 'Healthtech' is utilising HBM’s PW10 load cells to give improved accuracy, better design and to reduce manufacturing costs.

High-capacity scales

ELC: Robust Load Cell with Maximum Capacities From 220 kg to 1.76 t
Its robust design and the load cell's special cable make it fit for use in many different applications. The ELC load cell provides an accuracy of 1%.

RTN
Ideal for platform scales, truck scales, and tank weighing, the RTN Ring Torsion Load Cell from HBM covers a large rated load range from 1t to 470t.

S+P Wägetechnik GmbH
New mobile wireless scales by S+P remain operational for 4 weeks without recharging. This is due to the know-how and experience of HBM.

PW29
The hermetically encapsulated PW29 is a single point load cell for high maximum capacities and large weighing platforms.

Kolubara Metal
Measurement, weighing and determination of the center of gravity of mining machine superstructures using technology from HBM Test and Measurement.

Straightpoint
British load-testing specialist Straightpoint uses HBM strain gauges in all of its force measurement, load monitoring and load cell products.

Other OEM Applications

Strain Gauges for Transducer Manufacturers
Strain gauges available with various creep compensation values specifically designed for transducer manufacturing

Get the most out of TEDS (Transducer Electronic Data Sheet)
Learn how the TEDS technology makes the setup of a measurement chain reliable and fast in this webinar.

Selecting The Right Filter for Your Application

Infrastructure Monitoring

SLB700A/06VA
Active strain transducer with voltage or current output. Enabling in particular large forces to be measured in a cost efficient way.

M Series
Special strain gauge for high fatigue life at an extended strain level and high temperature gage up to 300°C.

Optical fiber sensors unveiled – How your needs can be fulfilled
In this webinar you will be guided through the fundamental concepts of optical fiber technology and how it can be used for sensing.

Optical and electrical test and measuring equipment in structural analysis
In this webinar, we will provide you with detailed information about hybrid measuring chains and, in particular, about the interface between the data acquisition system and the software

Webinar: Field installations of optical structural health monitoring systems: Lessons learned over more than a decade - April 27, 2017
In this webinar we would like to share with you our experience in installing systems based on this technology, the do’s and don’ts that we have listed over more than ten years.

Wind Turbine Testing with HBM
Wind turbine downtime involves high cost. HBM helps you identify mechanical stress on wind turbine components at an early stage.

KY Strain Gauge Chains for Determining Strain Gradients
KY strain gauge chains types consist of 10 or 15 very small measuring grids. Ideal choice for determining strain gradients.

VY Full Bridge Strain Gauges With 4 Measuring Grids For Tension/Compression Bars
VY full bridge strain gauges have 4 measuring grids, which are arranged so that each is offset to the next at an angle of 90°.

RY Strain Gauge Rosettes with 3 Measuring Grids
These strain gauges are an appropriate choice for analyzing the biaxial stress state with unknown principal strain directions.

DY Strain Gauges with 2 Parallel Measuring Grids
Double strain gauges with 1 measurement grid. Typical applications for these strain gauges include measurements on bending beams

XY2 XY4 Torsion/Shear Strain Gauges with 2 Measuring Grids
Types XY2 and XY4 are V-shaped strain gauges with 2 measuring grids arranged at an angle of about 45° to the axis.

XY T Rosettes with 2 Measuring Grids for Analyzing Biaxial Stress States
HBM XY strain gauges of the T rosettes type have 2 measuring grids arranged at a 90 degree angle offset from each other.

LY Linear Strain Gauges with 1 Measuring Grid
Linear strain gauges with 1 measurement grid is the first choice for strain measurements in only one direction.

C Series
Special strain gauge for the extended temperature range of -269°C to +250°C

Weldable Optical Strain Gauge Rosette OR-W
Robust strain gauge rosette based on Fiber Bragg Grating (FBG) technology to be spot welded on steel structures and materials exposed to harsh environments. Measures strain in three directions

Optical Acceleration Sensor FS65
Robust vibration sensor based on Fiber Bragg Grating (FBG) technology for measuring low frequency and small amplitude vibrations in a wide range of monitoring applications

Optical Tilt Sensor FS64
Ruggedized tilt sensor based on Fiber Bragg Grating (FBG) technology that measures angle variations towards the vertical in several applications (e.g. slopes and bridge pillars)

Optical Fiber Sensors vs. Conventional Electrical Strain Gauges for Infrastructure Monitoring Applications
Virtually every type of public infrastructure, including bridges, pipelines, tunnels, foundations, roadways, dams, etc., is subject to factors that can degrade it or lead to malfunctions. These structural problems can be the result of deterioration, improper construction methods, seismic activity, nearby construction work, etc.

Optical Temperature Sensors FS63
High-performance temperature sensors based on Fiber Bragg Grating (FBG) technology for measuring applications in large structures and electrical machines

Optical Strain Sensors FS62
High performance strain sensors based on Fiber Bragg Grating (FBG) technology for structural health monitoring in large structures and testing in laboratory applications

I.A.T. & Earthsystem: Monitoring of a church
The 18th century church of Santa Maria del Suffragio in Italy was destroyed by an earthquake in 2009. As it's being reconstructed, optical fiber sensors are used to monitor the structure.

Optimize your Structures with AHM (Asset Health Monitoring) Systems Based on Proven Sensor Technologies
This webinar explores the world of Asset Health Monitoring: See examples and learn about the HBM approach to this application with optical and electrical sensors.

Residual Stress Analysis Using the Hole Drilling Method
This webinar presents the hole drilling method for residual stress analysis using the high speed drilling method.

Infrastructure Monitoring with Optical Fiber Sensors: Different, not Difficult
This webinar is about the HBM FiberSensing experience using Fiber Bragg Grating systems in infrastructure monitoring applications.

Structural Health Monitoring (SHM) on Wind Turbines: Monitoring Systems for Rotor Blades, Towers and Foundations
The focus of this webinar is on monitoring systems for rotor blades, towers and foundations of wind turbines to extend their life time.

Resonant Bending Fatigue Test on Pipes

How to get the most out of your optical interrogator
In this HBM webinar, the Smart Peak Detection (SPD) method that allows the accurate detection of all sensors in large optical networks is explained.

Tunnel monitoring with Fiber Bragg sensors
How fiber optic sensors based on Fiber Bragg technology improve safety in tunnel monitoring.

LD20
Use of LD20 is recommended wherever high strain or compression occurs (>5 %). The SG has a maximum elongation of +/- 100,000 µm/m (+/-10 %).

LE11
The encapsulated strain gauge LE11 from HBM is oisture proof and resistant against chemicals.

LI66
The increased use of fiber composites and the systematic optimization of components presuppose a precise knowledge of the load situation.

XY / RY
HBM offers you strain gauges for analysis of residual stress and for the ring-core method as well as the hole drilling method.

LS31
The LS31 is a weldable strain gauge (SG) for measurements at elevated temperatures on weldable components and for use

RDS
HBM crack propagation gauges are used to determine crack propagation in a component. HBM offers three different types.

Weldable Optical Strain Gauge OL-W
Robust strain gauge based on Fiber Bragg Grating (FBG) technology suited for high strain applications. To be spot welded on steel structures and materials exposed to harsh environments.

What is a Fiber Bragg Grating?
A fiber Bragg grating is just a few millimeters long, highly sensitive and very reliable. Learn more about its properties!

Capturing data makes bridges last longer
Minho University is undertaking a long-term project to improve the durability of Portuguese bridges by using HBM’s equipment to monitor permanently fitted sensors.

Strukton
To monitor 24/7 that there is no danger of subsidence Avenue2 in Masstricht, HBM has installed strain gauges.

When the earth rocks... vibrating table tests at ZAG
When the earth rocks... vibrating table tests at ZAG

Structural Health Monitoring
The monitoring of structures helps detect changes in early stages, to avoid damages and to save money. HBM offers an intelligent and modular solution for efficient structural health monitoring.

Optical Fiber Sensors Unveiled – How These Sensors Will Fulfill your Application Needs (US)
In this webinar, you will be guided through the fundamental concepts of optical fiber technology and how it can be used for sensing.

Plant safety monitoring at EDF
HBM provided measurement equipment and services for monitoring a pressure pipe in a hydroelectric plant in France.

Holmenbrua
Examinations by HBM of the Holmenbrua bridge in Drammen in Norway was exposed to or whether improvements were needed.

Marti/Bitterli/EMPA
HBM force transducers are applied in a research project to reduce vibration in ultra-light belt conveyor galleries.

Monitoring El Giraldillo in Seville
A monitoring system including HBM's MGCplus amplifier system was used to monitor any mechanical changes to the sculpture during restoration work.

Calibration

Z30A Force Transducer for Challenging Calibration Tasks
The Z30A force transducer is designed for use as a reference standard for verification of calibration machines, and many other precision measurement tasks.

MGCplus - The renowned scalable and configurable data acquisition system for laboratory and test stand
The ultimate, scalable and configurable data acquisition system, for laboratory and test stand use, achieving acceptance as a measurement standard.

Torque Calibration
Precision at its best: HBM is offering you advanced torque calibration facilities for your torque sensors up to 400 kNm.

Force Calibration at HBM: From 2.5 N to 5 MN
Benefit from the proven precision of the HBM calibration laboratory when it comes to calibrating your load cell.

Building up reference measuring chains out of calibration transducers for force
In this webinar we explain the use and design of reference measuring chains based on calibration transducers. Learn what transducers are particularly suited for this application, how to choose the right calibration unit and what to keep in mind in terms of measurement uncertainty.

Article: Which calibration is the right one?
Sensor calibration is a sound investment in the future. There are different types of calibrations available. Which type of calibration to choose mainly depends on your requirements. This article explains the options.

Webinar: Ensure minimal measurement uncertainty: Everything you need to know about setting up a reference measurement chain for calibration - February 24, 2017
The webinar provides a general introduction to transducers and precision instruments including recommendations on measurement uncertainty and long-term stability.

TTS Transfer Torque Wrench For Calibration
Used to check and calibrate torque wrench calibration equipment, and offers extreme resistance to bending moments. Accuracy class 0.5 according to DKD‐R 3‐7.

TN Torque Transfer Normal
Non-rotating torque transducer specifically for use as a transfer standard or as a reference transducer in calibration laboratories.

TB2 Torque Reference Transducer With Extreme Accuracy
Torque reference transducer which was developed as a reference and transfer transducer for use in on-site calibration.

Z4A
High-precision transducer for reference measurement chains

TOP-Transfer
Reference force transducer offering maximum precision. Exceeds ISO376 requirements partly by a factor of 10.

BU18 Build-Up System for Extended Calibration Limits
Reference force transducer for compressive force, ISO376 class: 00 comprising three C18/1MN that can also be used individually

C18
For stationary and mobile use. Insensitive to humidity effects and rugged cable routing.

U15 Precision Load Cell: The Cost-Effective Reference Sensor
The amazingly cost-effective U15 precision load cell is ideally suited for use both as a transfer standard and as a reference sensor in calibration machines.

Torque measurement uncertainty 101
This webinar provides methods to calculate the measurement uncertainty in a torque measuring chain.

How to Reduce Measurement Uncertainty Throughout the Entire Force Measurement Chain
The webinar will explain the main aspects of measurement uncertainty along the complete force measurement chain – from real sensor to digital data stream.

Strain gage ¼ bridge calibration with shunt signals
Strain gage ¼ bridge calibration with shunt signals

Suggestions on how to include the effect of reproducibility in the evaluation of simplified calibration procedures
Suggestions on how to include the effect of reproducibility in the evaluation of simplified calibration procedures

Investigation of the influence of transducer electronic data sheets (TEDS) on calibration results
The international standard IEEE 1451.4 is the basis for transducer electronic data sheets (TEDS), where information related to the transducer like serial number or nominal sensitivity is stored into a chip inside the transducer. For bridge type sensors, with a novel circuit (patent pending) it is possible to read the TEDS information for 6-wire bridge sensors without additional wires by using the sense lines.

Guidelines for the determination of calibration intervals
Strictly seen: A calibration is only valid at the time of implementation. In practice, the question more frequently posed is how often should a recalibration actually be carried out. In general, the operator is responsible for the determination of calibration intervals.

Service, Training, Repair

DB Systemtechnik: Measurement technology in railway engineering
The European Dynotrain research project investigates to what extent computer simulations could replace part of the measurement runs in future.

Building up reference measuring chains out of calibration transducers for force
In this webinar we explain the use and design of reference measuring chains based on calibration transducers. Learn what transducers are particularly suited for this application, how to choose the right calibration unit and what to keep in mind in terms of measurement uncertainty.

Kolubara Metal
Measurement, weighing and determination of the center of gravity of mining machine superstructures using technology from HBM Test and Measurement.