Press Releases Archive
Deformación
Galgas extensométricas para análisis de tensiones
Galgas extensométricas para transductores
Sensores de fibra óptica
Accessorios para galgas extensométricas
Carga
Células de carga
Células de carga monoplato
Células de carga tipo viga a flexión
Células de carga digitales
Electrónica industrial
Fuerza
Sensores de fuerza
Sensores multieje
Sensores de fuerza piezoeléctricos
Par
Sensores de par
Sensores OEM
Sensores OEM a medida
Otros sensores
Sensores de presión
Sensores de desplazamiento
Transductores de corriente
Sondas de alta tensión
TEDS (Hojas de datos electrónicas de transductores)
Micrófonos
Acelerómetros
Sistemas de adquisición de datos
QuantumX – Universal
SomatXR – Robusto
MGCplus – Alto número de canales
Interrogadores ópticos
Genesis HighSpeed
Software y controladores
catman – Universal
catman Enterprise – Alto número de canales
Perception – HighSpeed
Driver y API para sistemas de adquisición de datos
Driver y API para Genesis HighSpeed y Perception
Automatización abierta - Software industrial, API y soluciones web
Analizadores de potencia
eDrive / eGrid Analizadores de potencia
Alta tensión Sistemas de ensayos y aislamiento
Base de conocimiento ensayos potencia eléctrica
PMX Adquisición de datos industrial
ClipX Acondicionador de señal
DSE Electrónica digital para sensores
Electrónica industrial y de pesaje Amplificadores y transmisores
Instrumentos de precisión
DMP41 Amplificador de precisión
Instrumentos de referencia Instrumentos de calibración
HBK Benelux – will work in close collaboration with the Brüel & Kjaer distributor in Benelux – ENMO Sound & Vibration Technology.
HBM unveils a specially designed, high-speed torque transducer.
(Darmstadt, November 2020) Further development of a testing and measuring portfolio does not necessarily mean new products – substantial progress and improved cost-effectiveness can also be attained by the evolution of established sensors. Hottinger Brüel & Kjær has proven this with the facelift of the configurable C10 compressive force transducer:
To help manufacturers of PCBs avoid damage or failure of their products, HBK has launched a Printed Circuit Board (PCB) Test Kit to detect weaknesses during the early stages of development.
Darmstadt, November 2020, World leading sensor manufacturer Hottinger Brüel & Kjær has launched a new addition to its MCS10 Multicomponent Sensor line from HBM - MCS10-200.
HBM has launched a new weighing terminal to expand the WTX series – the WTX110-D. The new addition to the portfolio can be connected to up to 32 digital load cells and is ideal for applications in truck and silo scales.
HBK has launched its latest virtual training course line up to provide a wide range of test and measurement know-how for engineers, acousticians and consultants.
To improve its mountaineering equipment, outdoor specialist, Simond used force transducers to develop safer, more reliable mountain climbing equipment.
Test and measurement specialist, HBK has launched the countdown to its virtual Product Physics Conference, taking place from 13th to 15th October 2020.
La nueva serie C11 de HBM está formada por transductores de fuerza de compresión con diseños ultraminiaturizados y una extraordinaria resistencia a la temperatura, que abren nuevos campos de aplicación. En cooperación con Kyowa.
May 2020 - To help customers grow their knowledge during these uncertain times, test and measurement specialist, HBM has created a bigger range of its webinar tutorials.
Ahora, los sensores de fuerza C9C y U9C de HBM también se comercializan con un amplificador de medida integrado, con conexión permanente. Este diseño simplifica enormemente la puesta a punto de la cadena de medida, ya que no es necesario soldar o crimpar, ni tampoco configurar un amplificador.
January 2020 - HBM has launched its 2020 training calendar, providing a range of theoretical and technical courses, designed to help engineers and consultants get the most from their tools.
HBM presenta su nuevo anillo de medida de fuerzas KMRplus, muy eficaz en tareas de medición de fuerza en entornos de producción e idóneo para funciones de monitorización.
February 2020 - Test and measurement specialist, HBM’s latest batch of webinars are now available for registration.
To help engineers avoid costly downtime and equipment damage, the HBM Academy provides a range of online training courses to help attendees get the most from their tools.
Carrying out reliable pressure tests within confined areas, such as gearboxes or coolant systems, is now a much simpler process for engineers with the launch of HBM’s miniature pressure transducer series - P60.
catman Enterprise es el software de adquisición de datos (DAQ) líder en ensayos con alto número de canales. Es una solución ideal para aplicaciones aeroespaciales, como ensayos estáticos y de fatiga de materiales. Ahora, con la versión 8.0 de catman Enterprise, es posible adquirir todo tipo de datos de buses de aviónica digitales, como ARINC-429 y MIL-STD-1553. Esta compatibilidad abre todo un nuevo campo de posibilidades de ensayo en el que los usuarios pueden beneficiarse de la experiencia de HBM con grandes volúmenes de canales. Desde ensayos de subsistemas —por ejemplo, trenes de aterrizaje— hasta pruebas Iron Bird a escala real.
Selecting the correct cable for a force measurement task can be a challenge. HBM has launched its new K-CAB-F connection cables, designed to simplify the process.
Following the initial announcement, in April 2018, of the merger between Hottinger Baldwin Messtechnik (HBM) and Brüel & Kjær, HBM’s Senior Vice President Product Management, Marketing and Strategy Thomas Lippok at HBM, provides an update on the latest developments.
Se ha utilizado tecnología óptica y de galgas extensométricas de HBM en la rehabilitación del puente suspendido más largo de Brasil, con el fin de garantizar la seguridad de los peatones y vehículos que cruzan a diario esta estructura de más de 90 años.
HBM presenta su primer acondicionador de señal de la serie ClipX con un servidor OPC UA integrado. Utiliza comunicación M2M para transmisión directa de datos de sensores a una nube con fines de análisis.
newLight es una línea de sensores ópticos de fácil instalación para medir deformación, inclinación, temperatura y aceleración. Los productos de esta línea utilizan tecnología de red de Bragg en fibra (FBG), reflejan los avances en la medición óptica y amplían las ventajas de la anterior gama de productos ópticos de HBM con una oferta exhaustiva de sensores ópticos.
HBM ha ampliado su catálogo de módulos de adquisición de datos con el nuevo módulo MX471C con protocolo CAN FD (CAN con velocidad de transferencia de datos flexible). Este módulo forma parte de las series QuantumX y SomatXR, todo un estándar industrial que ofrece a los ingenieros soluciones universales y flexibles para integrar sus sistemas de adquisición de datos en redes CANbus.
La nueva serie PACEline CFTplus de transductores de fuerza piezoeléctricos es la elección perfecta para hacer mediciones en los sectores de producción y fabricación. Los sensores CFTplus son especialmente idóneos para cubrir rangos de medida muy amplios; por ejemplo, en aplicaciones con prensas.