Webinar: Multi-channel data acquisition with high sample rate requirements – How to solve the challenge of high data throughput

Su cuenta en HBM.com

Actualización del registro de usuarios a partir del 17de junio de 2016

***Si ya tiene claves de acceso a HBMshop, puede utilizar la misma información para acceder a HBM.com

The webinar will explain the usage of a modular and scalable data acquisition system for fast measurements of electrical and mechanical quantities. You will learn how to use a modern data acquisition system as a transient recorder and data recorder at the same time. In addition, the following questions will be answered:

  • How can I solve data throughput limitations of standard network connections to be able to measure with extremely high sample rates?
  • How can I synchronize several distributed devices?

This webinar was recorded on November 23, 2016.

Presenter:

Dirk Eberlein

Dirk Eberlein

  • Since 2011: Product manager Perception and Genesis HighSpeed
  • 1998 - 2011: Application engineer and product manager for strain gauges
  • dirk.eberlein@hbm.com