Measurement of Resolver Position using Genesis Data Recorders

The resolver is an electrical machine that is intensively used in synchronous motor drives to measure the rotor position that is needed for the motor control algorithm. Due to its robustness, the resolver is the popular choice in harsh environments, where the electrical motor is subjected to mechanical stresses and vibrations, such as automotive and aerospace applications. The measured position is usually obtained through a resolver-to-digital converter that implements in a single chip several blocks, such as a signal demodulator, a voltage-controlled oscillator and a tracking loop. This work presents a method to obtain the position measured by a resolver using the high-speed voltage acquisition channels of HBM Genesis data recorders, with no requirement of additional hardware.

Contáctenos Contacte con HBM si desea saber más sobre lo que HBM le puede ofrecer.