Webinar: Calculating Residual Stress from the Measured Strain

Su cuenta en HBM.com

Actualización del registro de usuarios a partir del 17de junio de 2016

***Si ya tiene claves de acceso a HBMshop, puede utilizar la misma información para acceder a HBM.com

This webinar has been recorded and was originally held on September 21, 2018. Please login to access the recording.

One of the most crucial points when doing a residual stress analysis is the calculation of the results, starting from the measured strains. The hole drilling method provides a very well-known calculation in accordance with the ASTM E837 standard. There are also additional options that have been developed in recent years, each one having advantages and disadvantages. This webinar will provide some suggestions and hints to improve the calculation of the residual stress by hole drilling, with some practical examples and a focus on the typical uncertainty of this type of analysis.

Related products

Webinars
Looking for measurement technology news, useful information or tips & tricks? HBM offers an extensive choice of recorded webinars.
Events & Seminars
The HBM Academy offers seminars and trainings for all knowledge levels from beginner to measurement application professional.