StarkStrom Augsburg e.V. StarkStrom Augsburg e.V. | HBM

StarkStrom Augsburg e.V. Performs Chassis Measurements Using Strain Gauges From HBM

StarkStrom has so far determined chassis forces through calculations, simulations, and approximate reference values derived from the experience of the previous seasons. However, since reality can often differ from theory, we wanted to use strain gauges (SG) to determine the actual forces during several test drives. HBM has generously supported us in this process, with both the required components and specialist knowledge.

Over 20 strain gauges were installed on the individual chassis tubes. Due to the additional insulation layer, the weather caused no restrictions during the test runs. The results from the test runs are summarized below.

Real tie-rod load data during driving was required to be able to professionally design the autonomous steering of the autonomous UASA 1906-DV vehicle, "Fenja". Data was also required to validate the vehicle’s chassis design. This was achieved using the strain gauges provided by HBM.

The right half of the chassis was replaced by a measuring chassis. The aluminum chassis parts went through a calibration cycle on a tensile force machine before use. The cycle consisted of cyclic settling loads and subsequent loading in a step function to obtain a strain-force curve of the individual rods. The measured data obtained by the strain gauges and the tensile force machine were assigned using MATLAB.

The chassis was subsequently installed, adjusted, and measured. Highly dynamic maneuvers at the upper-performance limits had to be carried out to obtain meaningful results. For this purpose, several tracks were set up to cover all driving situations. Acceleration (75m straight acceleration), brake test (emergency braking from approx. 50km/h), skidpad (a horizontal eight), and a longer circuit were tested. Using the mobile analysis unit, memory unit, and battery together provided the optimal solution. We were able to carry the complete measuring equipment in the vehicle and record everything. Thus, measurements could be carried out under real conditions, which made the results highly relevant.

The test results were also processed using MATLAB. Several scripts were written to scale the measurement results of the strain-gauge measurements with those of other sensors, such as the steering angle or the x and y accelerations. This enabled us to illustrate the behavior of the vehicle in different situations.

The results obtained from the measurements were used as the basis for the design of the new autonomous steering system and durability simulations of chassis components. Furthermore, strain gauges were attached to the rear spoiler to verify CFD simulations and obtain information about the behavior of the aerodynamic package. The recorded data is currently being prepared for the validation of the previous chassis design.

The next step is to equip our electric racing car with a measuring chassis and strain gauges as well. This and the data from future measurements with the autonomous vehicle will be used to validate and improve our overall vehicle simulation. We also hope to achieve significant improvements in the design of the new chassis based on the results of the tests and simulations. In the future, we will be able to optimally vary the tube diameters and thicknesses and draw on practically proven results in the design judging.

The StarkStrom team would like to thank HBM for their support. A few results are shown in the following figures.

 



Exciting challenges are waiting for you!

HBM offers numerous opportunities for students, including internships or student trainee activities. Find out more about the various tasks and job offers.

Go to our career pages to find helpful tips for your application.

Interested?

You’ll find further exciting topics on our social media channels