Articles, Blog Posts & Tech Notes on Electric Power Testing

Your access to white papers, webinars, and videos is just one click away: start registering with your email address in order to get immediate access. 

Blog Posts

5 Tips for Selecting the Right Power Analyzer

Power analysers are multi-functional devices designed to measure the power flow in electrical systems. Although these sophisticated instruments are used in many applications and industries, there is no universal solution to every power measurement challenge. Find out what to consider when selecting a power analyzer that fits your application needs.

Más información

Blogpost: An Introduction to Electric Power Testing

Electric power testing gives in-depth analysis into the behaviour of the inverter, the motor and electric drive train. It can be quite complex and requires a real-time power analyser for high channel counts, dynamic load changes, raw data acquisition and advanced analysis. Electrical motor and inverter testing can be found in automotive, transportation, railways, aerospace, industrial, wind energy and also in power generation. Typical application areas are electric ship motor, electric fork lifter, wind energy generator, electric or hybrid car, high speed train, high-performance pumps, electric drive in Airbus A320, industrial VF inverter, multiphase AC industrial motor and much more.

Más información

¿Qué es un analizador de potencia?

Los analizadores de potencia permiten medir el flujo de potencia (w) en un sistema eléctrico. Este concepto se refiere a la tasa de transferencia eléctrica entre una fuente de energía y un pozo. Por eso, la potencia también se expresa alternativamente como energía por segundo (J/s). La medición del flujo de potencia es un proceso crítico, aunque rudimentario, que se puede llevar a cabo con suma facilidad utilizando un analizador de potencia estándar. Los sistemas más avanzados adquieren señales eléctricas, realizan cálculos integrados y llevan a cabo análisis adicionales complejos.

Más información

White Papers

Challenges in Testing Electric and More Electric Aircraft Motor and Inverters

The HBM eDrive power analyzer has unique features which make it an ideal measurement system for developing and validating electric aircraft powertrain. The eDrive solution simplifies testing complexity, allows users to test more quickly and gives a high level of traceability to tests. It does this by recording continuous data for large numbers of electrical and mechanical channels, then processes the data in real time to conduct power and efficiency calculations.

Dynamic Motor Power Measurement Enables In-Vehicle Testing of EVs

In-vehicle testing provides engineers with a method to benchmark competitors’ vehicles, calibrate drivetrains, and validate the performance of the product. In the emerging electric vehicle market, electrical power measurements on motors and related power conversion circuitry are becoming necessary to perform an evaluation of a vehicle. Mobile power measurement was previously difficult due to the dynamic nature of the vehicle speed. However, unique features provided in HBM’s eDrive, a system for testing electric machines and drives, make mobile electrical power measurements possible in real-world operating environments

Determinación de los parámetros del diagrama de circuito equivalente de un transformador

Los transformadores tienen numerosas aplicaciones y figuran entre los componentes más importantes de la tecnología de corriente alterna. Sirven para pasar energía eléctrica de un nivel de tensión a otro distinto. Para que la transmisión de la energía resulte eficaz, se requiere una buena eficiencia y una utilización óptima.

Caracterización y verificación de baterías de alta potencia

Antes de introducir en el mercado una batería de tracción, es imprescindible un proceso exhaustivo de caracterización y verificación. Para ello se requiere un banco de ensayos con un rango muy amplio de tensión y corriente, además de excelentes características dinámicas, para llevar a cabo las pruebas necesarias, de la manera más realista y orientada a la aplicación que sea posible.

Cálculos de potencia eléctrica con el software Perception

La evaluación y las pruebas de sistemas de accionamiento eléctricos para aplicaciones industriales y vehículos híbridos y eléctricos requieren mediciones de potencia precisas y muy dinámicas. Este artículo repasa los parámetros de potencia más importantes, con algunos ejemplos.

Mapas de eficiencia y pérdidas en motores de corriente alterna

En los últimos tiempos, las máquinas eléctricas son una temática importante para muchas industrias, como las de generación de energía, calefacción/refrigeración, transporte y electrodomésticos. Las normas sobre eficiencia se han endurecido y, al mismo tiempo, ha aumentado el número de dispositivos alimentados por batería. Todo ello ha puesto en primer plano la cuestión de la eficiencia de los motores.

Obtención de la constante de fuerza contraelectromotriz en motores de imanes permanentes

Para analizar con rapidez prototipos de nuevos motores de imanes permanentes es necesario identificar sus parámetros. Esta identificación de parámetros puede realizarse mediante pruebas complejas que utilizan un inversor y un mecanismo de accionamiento, o bien empleando métodos más sencillos, sin inversor ni accionamiento primario.

Mediciones de potencia en un motor de 6 fases

Para evaluar y probar motores eléctricos, y para implementar las correspondientes estrategias de control en las aplicaciones de movilidad eléctrica e industrial, se necesitan mediciones de potencia precisas y altamente dinámicas.

Mediciones de potencia con el software Perception en un inversor con modulación por ancho de pulsos

La evaluación y las pruebas de sistemas de accionamiento eléctricos para aplicaciones industriales y vehículos híbridos y eléctricos requieren mediciones de potencia precisas y muy dinámicas. A la hora de evaluar estos resultados de medición se debe tener en cuenta el modo de funcionamiento de los componentes del sistema de accionamiento.

Medida de la posición de un resolutor con registradores de datos Genesis HighSpeed

Un resolutor (resolver) es una máquina eléctrica muy utilizada en motores síncronos para medir la posición del rotor. Esta posición es necesaria para el algoritmo de control del motor. Los resolutores son robustos y, por ello, son una buena alternativa en entornos difíciles, en los que el motor está sometido a tensiones mecánicas y vibraciones, como ocurre en las aplicaciones de las industrias automovilística y aeroespacial.

Cálculo de las magnitudes de los vectores espaciales y el momento del entrehierro en motores asíncronos

Los registradores de datos Genesis HighSpeed, de HBM, resultan especialmente aptos para las mediciones en motores de inducción de corriente alterna alimentados mediante inversores. Gracias a su diseño modular, estos sistemas de medición permiten configurar cualquier número de canales con una elevada velocidad de muestreo.

Cálculo y representación de magnitudes medidas eléctricas como vectores espaciales mediante el software Perception de HBM

Los vectores espaciales se utilizan con frecuencia para representar de forma clara y concisa magnitudes medidas en sistemas de conversión de energía eléctrica, como transformadores o motores de inducción. Cuando estos vectores espaciales dependientes del tiempo se representan en el plano complejo, es posible obtener información adicional relativa al estado de funcionamiento de estos convertidores de energía.

Measurement of Symmetrical Components in Three-phase systems

The growing proportion of renewable energy requires these energy producers to also achieve high reliability and defined behavior in critical operating situations. The symmetrical components method can be used to assess and evaluate the operating points of renewable energy producers.

Become Part of the e-Power Community and Receive Tips and Tricks On How to Optimize Your Test Setup

You May Be Interested in ...