CONFIG_ADM6996_PHY=y
CONFIG_AR8216_PHY=y
# CONFIG_ATMEL_PWM is not set
CONFIG_CLKDEV_LOOKUP=y
CONFIG_FSNOTIFY=y
CONFIG_HAVE_MACH_CLKDEV=y
CONFIG_HW_HAS_PCI=y
CONFIG_INPUT=y
CONFIG_INPUT_EVDEV=y
# CONFIG_INPUT_GPIO_BUTTONS is not set
CONFIG_INPUT_POLLDEV=y
CONFIG_IRQ_FORCED_THREADING=y
# CONFIG_ISDN is not set
CONFIG_LANTIQ_ETOP=y
# CONFIG_LANTIQ_MACH_ARV is not set
# CONFIG_LANTIQ_MACH_EASY50712 is not set
CONFIG_LANTIQ_MACH_FRITZ_AR9=y
# CONFIG_LANTIQ_MACH_FRITZ_VR9 is not set
# CONFIG_LANTIQ_MACH_GIGASX76X is not set
CONFIG_LANTIQ_MACH_NETGEAR=y
CONFIG_LANTIQ_MACH_WBMR=y
CONFIG_LANTIQ_MACH_P2601HNFX=y
CONFIG_LANTIQ_MACH_H201L=y
# CONFIG_LANTIQ_VRX200 is not set
CONFIG_MDIO_BOARDINFO=y
CONFIG_MTD_BLOCK2MTD=y
CONFIG_PCI=y
# CONFIG_PCIEPORTBUS is not set
# CONFIG_PCIE_LANTIQ is not set
CONFIG_PCI_DOMAINS=y
CONFIG_PCI_LANTIQ=y
# CONFIG_PCI_LANTIQ_NONE is not set
CONFIG_RTL8306_PHY=y
# CONFIG_SOC_AMAZON_SE is not set
# CONFIG_SOC_FALCON is not set
CONFIG_SOC_TYPE_XWAY=y
CONFIG_SOC_XWAY=y
# CONFIG_SOC_SVIP is not set
CONFIG_USB_ARCH_HAS_XHCI=y
CONFIG_USB_SUPPORT=y