2013-07-28  Tobias Burnus  <burnus@net-b.de>

	Backport from mainline
	2013-05-28  Dominique d'Humieres  <dominiq@lps.ens.fr>

	PR fortran/57435
	* module.c (check_for_ambiguous): Avoid null pointer deref.

2013-07-08  Tobias Burnus  <burnus@net-b.de>

	PR fortran/57785
	* simplify.c (compute_dot_product): Complex conjugate for
	dot_product.
	(gfc_simplify_dot_product, gfc_simplify_matmul): Update call.

2013-06-11  Tobias Burnus  <burnus@net-b.de>

	PR fortran/57508
	* resolve.c (get_temp_from_expr): Don't copy function
	result attributes to temporary.

2013-06-04  Tobias Burnus  <burnus@net-b.de>

	Backport from mainline
	2013-05-22  Tobias Burnus  <burnus@net-b.de>

	PR fortran/57364
	* resolve.c (get_temp_from_expr): Commit created sym.

2013-05-31  Janus Weil  <janus@gcc.gnu.org>
	    Tobias Burnus  <burnus@net-b.de>

	PR fortran/57217
	* interface.c (check_dummy_characteristics): Symmetrize type check.

2013-05-31  Release Manager

	* GCC 4.8.1 released.

2013-05-22  Janne Blomqvist  <jb@gcc.gnu.org>

	* intrinsic.texi (RANDOM_SEED): Improve example.

2013-05-07  Tobias Burnus  <burnus@net-b.de>

	Backport from mainline
	2013-05-02  Tobias Burnus  <burnus@net-b.de>

	PR fortran/57142
	* simplify.c (gfc_simplify_size): Renamed from
	simplify_size; fix kind=8 handling.
	(gfc_simplify_size): New function.
	(gfc_simplify_shape): Add range check.
	* resolve.c (resolve_function): Fix handling
	for ISYM_SIZE.

2013-04-26  Janus Weil  <janus@gcc.gnu.org>

	Backports from trunk:

	PR fortran/56814
	* interface.c (check_result_characteristics): Get result from interface
	if present.

	PR fortran/56968
	* expr.c (gfc_check_pointer_assign): Handle generic functions returning
	procedure pointers.

	PR fortran/53685
	PR fortran/57022
	* check.c (gfc_calculate_transfer_sizes): Fix for array-valued SOURCE
	expressions.
	* target-memory.h (gfc_element_size): New prototype.
	* target-memory.c (size_array): Remove.
	(gfc_element_size): New function.
	(gfc_target_expr_size): Modified to always return the full size of the
	expression.

2013-04-22  Thomas Koenig  <tkoenig@gcc.gnu.org>
	    Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/56872
	* frontend-passes.c (copy_walk_reduction_arg): Change argument type
	to gfc_constructor.  If it has an iterator, wrap the copy of its
	expression in an array constructor with that iterator.  Don't special
	case function expressions.
	(callback_reduction): Update caller.  Don't return early if there is
	an iterator.

2013-04-18  Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/56816
	* match.c (gfc_match_select_type): Add syntax error. Move namespace
	allocation and cleanup...
	* parse.c (decode_statement): ... here.

2013-04-18  Tobias Burnus  <burnus@net-b.de>

	PR fortran/56994
	* invoke.texi (NEAREST): S argument is not optional.

2013-04-08  Thomas Koenig  <tkoenig@gcc.gnu.org>

	PR fortran/56782
	Backport fron trunk.
	* frontend-passes.c (callback_reduction):  Dont't do
	any simplification if there is only a single element
	which has an iterator.

2013-03-22  Release Manager

	* GCC 4.8.0 released.

2013-03-15  Tobias Burnus  <burnus@net-b.de>

	PR fortran/56615
	* trans-intrinsic.c (gfc_conv_intrinsic_transfer): Pack arrays
	if they are not simply contiguous.

2013-03-11  Tobias Burnus  <burnus@net-b.de>

	* gfortran.texi (STRUCTURE and RECORD): State more clearly how
	to convert them into derived types.

2013-03-10  Paul Thomas  <pault@gcc.gnu.org>

	PR fortran/56575
	* expr.c (gfc_default_initializer): Check that a class declared
	type has any components.
	* resolve.c (resolve_fl_derived0): On failing the test for C437
	set the type to BT_UNKNOWN to prevent repeat error messages.

2013-03-03  Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/56477
	* expr.c (gfc_check_pointer_assign): Avoid NULL pointer dereference.

2013-03-03  Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/54730
	* array.c (gfc_match_array_constructor): Set a checkpoint before
	matching a typespec.  Drop it on success, restore it otherwise.

2013-03-03  Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/54730
	* gfortran.h (struct gfc_undo_change_set): New field 'previous'.
	(gfc_new_undo_checkpoint, gfc_drop_last_undo_checkpoint,
	gfc_restore_last_undo_checkpoint): New prototypes.
	* symbol.c (default_undo_chgset_var): Update initialization.
	(single_undo_checkpoint_p, gfc_new_undo_checkpoint,
	free_undo_change_set_data, pop_undo_change_set,
	gfc_drop_last_undo_checkpoint, enforce_single_undo_checkpoint):
	New functions.
	(save_symbol_data): Handle multiple change sets.  Make sure old_symbol
	field's previous value is not overwritten.  Clear gfc_new field.
	(restore_old_symbol): Restore previous old_symbol field.
	(gfc_restore_last_undo_checkpoint): New function, using body renamed
	from gfc_undo_symbols.  Restore the previous change set as current one.
	(gfc_undo_symbols): New body.
	(gfc_commit_symbols, gfc_commit_symbol, gfc_enforce_clean_symbol_state):
	Call enforce_single_undo_checkpoint.
	(gfc_symbol_done_2): Ditto.  Free change set data.

2013-03-03  Mikael Morin  <mikael@gcc.gnu.org>

	* symbol.c (restore_old_symbol): Fix thinko.

2013-03-03  Mikael Morin  <mikael@gcc.gnu.org>

	* symbol.c (gfc_undo_symbols): Move code...
	(restore_old_symbol): ... here as a new function.

2013-03-03  Mikael Morin  <mikael@gcc.gnu.org>

	* Make-lang.in (F95_PARSER_OBJS): Add dependency to vec.h.
	* gfortran.h: Include vec.h.
	(gfc_undo_change_set): New struct.
	* symbol.c (tentative_tbp): Remove struct.
	(changed_syms, tentative_tbp_list): Remove variables.
	(default_undo_chgset_var, latest_undo_chgset): New variables.
	(save_symbol_data, gfc_get_sym_tree, gfc_undo_symbols,
	gfc_commit_symbols, gfc_commit_symbol,
	gfc_enforce_clean_symbol_state, gfc_get_typebound_proc):
	Use latest_undo_chgset instead of changed_syms and tentative_tbp_list.

2013-03-01  Tobias Burnus  <burnus@net-b.de>

	PR fortran/56491
	* iresolve.c (resolve_bound): Use gfc_get_string instead of xstrdup.
	* symbol.c (free_components): Free proc-pointer components.

2013-03-01  Tobias Burnus  <burnus@net-b.de>

	* trans-decl.c (gfc_trans_deferred_vars): Free expr after use.
	* trans-io.c (build_dt): Ditto.

2013-02-24  Joseph Myers  <joseph@codesourcery.com>

	* resolve.c (generate_component_assignments): Don't use UTF-8
	ligature in diagnostic.

2013-02-21  Janus Weil  <janus@gcc.gnu.org>

	PR fortran/56385
	* trans-array.c (structure_alloc_comps): Handle procedure-pointer
	components with allocatable result.

2012-02-21  Tobias Burnus  <burnus@net-b.de>

	PR fortran/56416
	* gfortran.texi (Part II: Language Reference, Extensions,
	Non-Fortran Main Program): Sort @menu to match actual section order.
	* intrinsic.texi (Intrinsic Procedures): Ditto.
	(C_F_POINTER, PRECISION): Move to the alphabetically correct place.

2013-02-15  Tobias Burnus  <burnus@net-b.de>
	    Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/56318
	* simplify.c (gfc_simplify_matmul): Fix result shape
	and matmul result.

2013-02-15  Tobias Burnus  <burnus@net-b.de>

	PR fortran/53818
	* resolve.c (apply_default_init_local): Don't create an
	initializer for a result variable.

2013-02-14  Thomas Koenig  <tkoenig@gcc.gnu.org>

	PR fortran/56224
	* gfortran.h (gfc_add_include_path):  Add boolean argument
	for warn.
	* scanner.c (gfc_add_include_path):  Pass along warn argument
	to add_path_to_list.
	* options.c (gfc_post_options):  Add true warn argument to
	gfc_add_include_path.
	(gfc_handle_module_path_options):  Likewise.
	(gfc_handle_option): Also gfc_add_include_path for intrinsic
	modules, without warning.

2013-02-14  Paul Thomas  <pault@gcc.gnu.org>
	    Tobias Burnus  <burnus@net-b.de>

	PR testsuite/56138
	* trans-decl.c (gfc_get_symbol_decl): Fix deferred-length
	results for functions without extra result variable.

	Revert:
	2013-01-30  Tobias Burnus  <burnus@net-b.de>

	PR fortran/56138
	* trans-decl.c (gfc_trans_deferred_vars): Fix deferred-length
	results for functions without extra result variable.

2013-02-12  Janus Weil  <janus@gcc.gnu.org>

	PR fortran/46952
	* resolve.c (resolve_call): Do not check deferred procedures for
	recursiveness.

2013-02-09  Paul Thomas  <pault@gcc.gnu.org>

	PR fortran/55362
	* check.c (array_check): It is an error if a procedure is
	passed.

2013-02-08  Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/54107
	* trans-types.c (gfc_get_function_type): Change a NULL backend_decl
	to error_mark_node on entry.  Detect recursive types.  Build a variadic
	procedure type if the type is recursive.  Restore the initial
	backend_decl.

2013-02-07  Tobias Burnus  <burnus@net-b.de>

	PR fortran/54339
	* gfortran.texi (Standards): Mention TS29113.
	(Varying Length Character): Mention deferred-length
	strings.
	(Fortran 2003 Status): Add unlimited polymorphic.
	(TS 29113 Status): Add TYPE(*) and DIMENSION(..).
	(C Interop): Update the section about TS29113.

2013-02-06 Paul Thomas  <pault@gcc.gnu.org>

	PR fortran/55789
	* trans-array.c (trans_array_constructor): Remove condition
	'dynamic' = true if the loop ubound is a VAR_DECL.

2013-02-04  Paul Thomas  <pault@gcc.gnu.org>

	PR fortran/56008
	PR fortran/47517
	* trans-array.c (gfc_alloc_allocatable_for_assignment): Save
	the lhs descriptor before it is modified for reallocation. Use
	it to deallocate allocatable components in the reallocation
	block.  Nullify allocatable components for newly (re)allocated
	arrays.

2013-02-04  Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/54195
	* resolve.c (resolve_typebound_procedures): Recurse through
	resolve_symbol.

2013-02-04  Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/54107
	PR fortran/54195
	* gfortran.h (struct gfc_symbol): New field 'resolved'.
	* resolve.c (resolve_fl_var_and_proc): Don't skip result symbols.
	(resolve_symbol): Skip duplicate calls.  Don't check the current
	namespace.

2013-02-02  Thomas Koenig  <tkoenig@gcc.gnu.org>

	PR fortran/50627
	PR fortran/56054
	* decl.c (gfc_match_end):  Remove half-ready namespace
	from parent if the end of a block is missing.
	* parse.c (parse_module):  Do not put namespace into
	gsymbol on error.

2013-01-30  Tobias Burnus  <burnus@net-b.de>

	PR fortran/56138
	* trans-decl.c (gfc_trans_deferred_vars): Fix deferred-length
	results for functions without extra result variable.

2013-01-29  Janus Weil  <janus@gcc.gnu.org>
	    Mikael Morin <mikael@gcc.gnu.org>

	PR fortran/54107
	* gfortran.h (gfc_component): Delete members 'formal' and 'formal_ns'.
	(gfc_copy_formal_args,gfc_copy_formal_args_ppc,gfc_expr_replace_symbols,
	gfc_expr_replace_comp): Delete.
	(gfc_sym_get_dummy_args): New prototype.
	* dependency.c (gfc_check_fncall_dependency): Use
	'gfc_sym_get_dummy_args'.
	* expr.c (gfc_is_constant_expr): Ditto.
	(replace_symbol,gfc_expr_replace_symbols,replace_comp,
	gfc_expr_replace_comp): Deleted.
	* frontend-passes.c (doloop_code,do_function): Use
	'gfc_sym_get_dummy_args'.
	* interface.c (gfc_check_operator_interface,gfc_compare_interfaces,
	gfc_procedure_use,gfc_ppc_use,gfc_arglist_matches_symbol,
	gfc_check_typebound_override): Ditto.
	* module.c (MOD_VERSION): Bump module version.
	(mio_component): Do not read/write 'formal' and 'formal_ns'.
	* resolve.c (resolve_procedure_interface,resolve_fl_derived0): Do not
	copy formal args, but just keep a pointer to the interface.
	(resolve_function,resolve_call,resolve_typebound_generic_call,
	resolve_ppc_call,resolve_expr_ppc,generate_component_assignments,
	resolve_fl_procedure,gfc_resolve_finalizers,check_generic_tbp_ambiguity,
	resolve_typebound_procedure,check_uop_procedure): Use
	'gfc_sym_get_dummy_args'.
	* symbol.c (free_components): Do not free 'formal' and 'formal_ns'.
	(gfc_copy_formal_args,gfc_copy_formal_args_ppc): Deleted.
	(gfc_sym_get_dummy_args): New function.
	* trans-array.c (get_array_charlen,gfc_walk_elemental_function_args):
	Use 'gfc_sym_get_dummy_args'.
	* trans-decl.c (build_function_decl,create_function_arglist,
	build_entry_thunks,init_intent_out_dt,gfc_trans_deferred_vars,
	add_argument_checking): Ditto.
	* trans-expr.c (gfc_map_fcn_formal_to_actual,gfc_conv_procedure_call,
	gfc_conv_statement_function): Ditto.
	* trans-stmt.c (gfc_conv_elemental_dependencies): Ditto.
	* trans-types.c (create_fn_spec,gfc_get_function_type): Ditto.

2013-01-28  Tobias Burnus  <burnus@net-b.de>
	    Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/53537
	* symbol.c (gfc_find_sym_tree): Don't look for the symbol outside an
	interface block.
	(gfc_get_ha_symtree): Let gfc_find_sym_tree lookup the parent namespace.
	* decl.c (gfc_match_data_decl): Ditto.
	(variable_decl): Remove undeclared type error.
	(gfc_match_import): Use renamed instead of original name.

2013-01-27 Paul Thomas  <pault@gcc.gnu.org>

	PR fortran/55984
	PR fortran/56047
	* gfortran.h : Add associate_var to symbol_attr.
	* resolve.c (resolve_assoc_var): Set associate_var attribute.
	If the target class_ok is set, set it for the associate
	variable.
	* check.c (allocatable_check): Associate variables should not
	have the allocatable attribute even if their symbols do.
	* class.c (gfc_build_class_symbol): Symbols with associate_var
	set will always have a good class container.

2013-01-23  Janus Weil  <janus@gcc.gnu.org>

	PR fortran/56081
	* resolve.c (resolve_select): Add argument 'select_type', reject
	non-scalar expressions.
	(resolve_select_type,resolve_code): Pass new argument to
	'resolve_select'.

2013-01-23  Jakub Jelinek  <jakub@redhat.com>

	PR fortran/56052
	* trans-decl.c (gfc_get_symbol_decl): Set DECL_ARTIFICIAL
	and DECL_IGNORED_P on select_type_temporary and don't set
	DECL_BY_REFERENCE.

2013-01-21  Thomas Koenig  <tkoenig@gcc.gnu.org>

	PR fortran/55919
	* scanner.c (add_path_to_list): Copy path to temporary and strip
	trailing directory separators before calling stat().

2013-01-17  Richard Biener  <rguenther@suse.de>

	* trans-stmt.c (gfc_trans_do): Conditionally compute countm1
	dependent on sign of step, avoids repeated evaluation of
	step sign test.  Avoid undefined overflow issues by using unsigned
	arithmetic.

2013-01-16  Janus Weil  <janus@gcc.gnu.org>

	PR fortran/55983
	* class.c (find_typebound_proc_uop): Check for f2k_derived instead of
	asserting it.

2013-01-16  Jakub Jelinek  <jakub@redhat.com>
	    Tobias Burnus  <burnus@net-b.de>

	PR driver/55884
	* lang.opt (fintrinsic-modules-path): Don't accept Joined.
	(fintrinsic-modules-path=): New.
	* options.c (gfc_handle_option, gfc_get_option_string,
	gfc_get_option_string): Handle the latter.

2013-01-16  Jakub Jelinek  <jakub@redhat.com>

	PR fortran/52865
	* trans-stmt.c (gfc_trans_do): Put countm1-- before conditional
	and use value of countm1 before the decrement in the condition.

2013-01-15  Paul Thomas  <pault@gcc.gnu.org>

	PR fortran/54286
	* expr.c (gfc_check_pointer_assign): Check for presence of
	's2' before using it.

2013-01-14  Thomas Koenig  <tkoenig@gcc.gnu.org>

	PR fortran/55806
	* frontend-passes.c (optimize_reduction):  New function,
	including prototype.
	(callback_reduction):  Likewise.
	(gfc_run_passes):  Also run optimize_reduction.
	(copy_walk_reduction_arg):  New function.
	(dummy_code_callback):  New function.

2013-01-13  Jakub Jelinek  <jakub@redhat.com>

	PR fortran/55935
	* trans-expr.c (gfc_conv_structure): Call
	unshare_expr_without_location on the ctor elements.

2013-01-13  Paul Thomas  <pault@gcc.gnu.org>

	PR fortran/54286
	* expr.c (gfc_check_pointer_assign): Ensure that both lvalue
	and rvalue interfaces are presented to gfc_compare_interfaces.
	Simplify references to interface names by using the symbols
	themselves. Call gfc_compare_interfaces with s1 and s2 inter-
	changed to overcome the asymmetry of this function. Do not
	repeat the check for the presence of s1 and s2.

2013-01-12  Janus Weil  <janus@gcc.gnu.org>

	PR fortran/55072
	* trans-array.c (gfc_conv_array_parameter): No packing was done for
	full arrays of derived type.

2013-01-08  Paul Thomas  <pault@gcc.gnu.org>

	PR fortran/55868
	* class.c (get_unique_type_string): Change $tar to STAR and
	replace sprintf by strcpy where there is no formatting.
	* decl.c (gfc_match_decl_type_spec): Change $tar to STAR.

2013-01-09  Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/47203
	* module.c (check_for_ambiguous): Get the current program unit using
	gfc_current_ns.

2013-01-09  Tobias Burnus  <burnus@net-b.de>

	PR fortran/55758
	* resolve.c (resolve_symbol): Reject non-C_Bool logicals
	in BIND(C) procedures with -std=f*.

2013-01-08  Paul Thomas  <pault@gcc.gnu.org>

	PR fortran/55618
	* trans-expr.c (gfc_conv_procedure_call): Dereference scalar
	character function arguments to elemental procedures in
	scalarization loops.

2013-01-07  Tobias Burnus  <burnus@net-b.de>

	PR fortran/55763
	* gfortran.h (gfc_check_assign_symbol): Update prototype.
	* decl.c (add_init_expr_to_sym, do_parm): Update call.
	* expr.c (gfc_check_assign_symbol): Handle BT_CLASS and
	improve error location; support components.
	(gfc_check_pointer_assign): Handle component assignments.
	* resolve.c (resolve_fl_derived0): Call gfc_check_assign_symbol.
	(resolve_values): Update call.
	(resolve_structure_cons): Avoid double diagnostic.

2013-01-07  Tobias Burnus  <burnus@net-b.de>
	    Thomas Koenig  <tkoenig@gcc.gnu.org>

	PR fortran/55852
	* expr.c (gfc_build_intrinsic_call): Avoid clashes
	with user's procedures.
	* gfortran.h (gfc_build_intrinsic_call): Update prototype.
	* simplify.c (gfc_simplify_size): Update call.
	* class.c (finalization_scalarizer, finalization_get_offset,
	finalizer_insert_packed_call, generate_finalization_wrapper):
	Clean up by using gfc_build_intrinsic_call.

2013-01-07  Tobias Burnus  <burnus@net-b.de>

	PR fortran/55763
	* resolve.c (resolve_select_type): Reject intrinsic types for
	a non-unlimited-polymorphic selector.

2013-01-06  Paul Thomas  <pault@gcc.gnu.org>

	PR fortran/53876
	PR fortran/54990
	PR fortran/54992
	* trans-array.c (build_array_ref): Check the TYPE_CANONICAL
	to see if it is GFC_CLASS_TYPE_P.
	* trans-expr.c (gfc_get_vptr_from_expr): The same.
	(gfc_conv_class_to_class): If the types are not the same,
	cast parmese->expr to the type of ctree.
	* trans-types.c (gfc_get_derived_type): GFC_CLASS_TYPE_P of
	CLASS components must be set.

2013-01-06  Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/42769
	PR fortran/45836
	PR fortran/45900
	* module.c (read_module): Don't reuse local symtree if the associated
	symbol isn't exactly the one wanted.  Don't reuse local symtree if it is
	ambiguous.
	* resolve.c (resolve_call): Use symtree's name instead of symbol's to
	lookup the symtree.

2013-01-05  Steven G. Kargl  <kargl@gcc.gnu.org>
	    Mikael Morin  <mikael@gcc.gnu.org>

	PR fortran/55827
	* class.c (gfc_fix_class_refs): Adapt ts initialization for the case
	e->symtree == NULL.
	* trans-expr.c (gfc_conv_function_expr): Init sym earlier. Use it.

2013-01-05  Tobias Burnus  <burnus@net-b.de>

	* class.c (finalize_component): Used passed offset expr.
	(finalization_get_offset): New static function.
	(finalizer_insert_packed_call, generate_finalization_wrapper): Use it
	to handle noncontiguous arrays.

2013-01-04  Tobias Burnus  <burnus@net-b.de>

	* trans.c (gfc_build_final_call): New function.
	* trans.h (gfc_build_final_call, gfc_conv_scalar_to_descriptor):
	New function prototypes.
	* trans-expr.c (gfc_conv_scalar_to_descriptor): Renamed from
	conv_scalar_to_descriptor, removed static attribute.
	(gfc_conv_procedure_call): Honor renaming.

2013-01-04  Tobias Burnus  <burnus@net-b.de>

	* intrinsic.c (add_functions): New internal intrinsic
	function GFC_PREFIX ("stride").
	* gfortran.h (gfc_isym_id): Add GFC_ISYM_STRIDE.
	* intrinsic.h (gfc_resolve_stride): New prototypes.
	* iresolve.c (gfc_resolve_stride): New function.
	* trans-intrinsic.c (conv_intrinsic_stride): New static
	function.
	(gfc_conv_intrinsic_function): Use it.

2013-01-04  Tobias Burnus  <burnus@net-b.de>

	* class.c (gfc_find_intrinsic_vtab): Add _final
	component.
	* decl.c (gfc_match_null): Remove superfluous
	variadic argument to gfc_match.

2013-01-04  Paul Thomas  <pault@gcc.gnu.org>

	PR fortran/55172
	* match.c (copy_ts_from_selector_to_associate): Remove call to
	gfc_resolve_expr and replace it with explicit setting of the
	array reference type.
	* resolve.c (resolve_select_type): It is an error if the
	selector is coindexed.

2013-01-04  Tobias Burnus  <burnus@net-b.de>

	PR fortran/55763
	* decl.c (gfc_match_null): Parse and reject MOLD.

2013-01-04  Tobias Burnus  <burnus@net-b.de>

	PR fortran/55854
	PR fortran/55763
	* class.c (gfc_class_null_initializer): Fix finding the vtab.
	(gfc_find_intrinsic_vtab): Use BT_VOID for some components.

2013-01-03  Janus Weil  <janus@gcc.gnu.org>

	PR fortran/55855
	* expr.c (gfc_check_assign): Use 'gfc_expr_attr' to evaluate attributes
	of rvalue. Correct hyphenation in error message.

2013-01-03  Jakub Jelinek  <jakub@redhat.com>

	* gfortranspec.c (lang_specific_driver): Update copyright notice
	dates.

Copyright (C) 2013 Free Software Foundation, Inc.

Copying and distribution of this file, with or without modification,
are permitted in any medium without royalty provided the copyright
notice and this notice are preserved.